PA1445U-1CS4

Toshiba 14-inch Envoy Series Ballistic Polyester Carrying Case

Fits up to 14.1-inch laptop

MSRP: $44.99
Shop Online
Toshiba 14-inch Envoy Series Ballistic Polyester Carrying Case 4.75 out of 5.0 based on 4 user reviews. Average Customer Rating: 4.75 out of 5.0
Read Reviews (4)  | Write Reviews

Laptop Cases - PA1445U-1CS4 Customer Reviews

Great Case

POSTED BY: , Boston, MA
Overall rating: 5.0 out of 5

"I just returned from a two week business trip wtih this case. The trip involved, airports, hotels and conferences and it was just what I needed. Besides having an excellent storage slot for my Toshiba it also has ample room for documents, pens, mouse, and power cord. A great product."

Great Bag

POSTED BY: , Riverdale, GA
Overall rating: 5.0 out of 5

"There was only one thing i did not like about this bag is that the compartment when the laptop goes does not zip down very far. not even half-way really, while is is not a problem for my computer, it might a problem for others. other than that it is really great, lots of space for just about anything reasonable. I would recommend this to a friend."

A very well-made case

POSTED BY: , NY Metro area
Overall rating: 4.0 out of 5

"This case is of excellent build quality. The laptop compartment is well-padded, the polyester is high quality, hardware is also good quality and the shoulder strap is well-padded. What prevented a 5 star rating for me was that the checkpoint friendly feature on mine was had a sticky zipper (could be an isolated incident) and I am personally not a big fan of top-loading laptop compartments I may be more picky than most on this but I get the feeling that the zippers can potentially scratch the laptop finish when placing and taking the laptop out of the compartment. I would prefer zippers that unzip further to avoid zippers from scraping against the laptop. That being said overall this case is the highest quality soft case that I have seen for a 14 inch laptop."

Excellent Computer Case for 14" Satellite

POSTED BY: , Tallahassee, FL
Overall rating: 5.0 out of 5

"I have searched all over and have come to the conclusion that this case is the best companion to the 14" Toshiba Satellite Notebook. It's versatility allows you to carry all the extras you may need."