PA1447U-1CS8

Toshiba 18.4-inch Lightweight Carrying Case

Fits up to 18.4-inch screen portables

MSRP: $44.99
Shop Online
Toshiba 18.4-inch Lightweight Carrying Case 4.43 out of 5.0 based on 7 user reviews. Average Customer Rating: 4.43 out of 5.0
Read Reviews (7)  | Write Reviews

Laptop Cases - PA1447U-1CS8 Customer Reviews

OK

POSTED BY:
Overall rating: 4.0 out of 5

"Holding strap broke after 2 weeks, I think it was defective and am waiting for the new one to arraive."

Best Laptop Case Ever

POSTED BY: , rome, ny
Overall rating: 5.0 out of 5

"It has a sleek fit, and gives you enough room for assecories without that bulky look."

Not very strong

POSTED BY:
Overall rating: 2.0 out of 5

"Had this laptop case for a few weeks, used it for my laptop. The laptop fit in there nicely, and it's a nice bag, but the strap broke within 3 weeks of using it. Very disappointed in the quality, especially for the price that I paid for the bag."

Very nice case

POSTED BY: , Kendallville, In
Overall rating: 5.0 out of 5

"I bought the computer as soon as it came out, I've been looking for a case since then. I'm picky when it comes to cases, this one has everything that I look for. It is made of very durable materials, plenty of padding, lots of compartments for everyting that you need, a case for the transformer. I've purchased Toshiba brand products and I've never been disapointed, the trend continues with this case. If you have an 18.4 laptop and want a great slim case this is the one that you need."

Excellent Bag for 18.4 Laptop

POSTED BY: , St. Louis, Mo.
Overall rating: 5.0 out of 5

"Could not be happier with this new bag, There are not too many bags for 18.4 inch size. I waited a year to find a bag like this. Perfect for large laptops. Very good quality, sturdy and well padded sides."

Toshiba 18.4" carry case is great!!!

POSTED BY: , Reeds Spring, MO
Overall rating: 5.0 out of 5

"It fits the Toshiba Qosmio 18.4 inch Laptop prefectly and in very well built. Has a great handle with padded shoulder and adjustable padding inside ensures a secure fit for your laptop. I love it. Great price too."

Definitely for Qosmio G55-Q804

POSTED BY: , San Diego, CA
Overall rating: 5.0 out of 5

"For those of you who have been looking for a bag for the Qosmio G55-Q804 and related models, don't look no further. Most likely, you have been looking all over to find a bag for this monster-size laptop. I spent many hours on the Internet and in computer stores without any luck. But this bag truly fits! The bag has a simple, yet high-quality design and does the job well. Inside, there is obviously a padded area for the laptop. In addition, two pockets have been added on the inside which are perfect for the adapter and mouse. There is also an outside pocket with zipper. The handle is really cool, as the two pieces slide into each other and give you a confident feel about carrying the bag."