PA1450U-1EB6

Toshiba 16-inch Lightweight BackPack

Fits up to 16” portable

MSRP: $29.99
Shop Online
Toshiba 16-inch Lightweight BackPack 3.00 out of 5.0 based on 4 user reviews. Average Customer Rating: 3.00 out of 5.0
Read Reviews (4)  | Write Reviews

Laptop Cases - PA1450U-1EB6 Customer Reviews

Worst Bag Ever

POSTED BY: , Santa ana
Overall rating: 1.0 out of 5

"I had a friend of mine order the bag for me and ive had it a little over 5 months and during this time the bag has completely fallen apart the zipper material had fallen off and the shoulder straps have started to rip off. i loved Toshiba laptops so this bag was kind of a let down."

Great Bag for the Money

POSTED BY: , nc
Overall rating: 5.0 out of 5

"This bag is well padded and has plenty of room for other items as well. Great bag for the money. I purchased two."

yes, there is a pouch inside.

POSTED BY: , San Francisco, CA
Overall rating: 5.0 out of 5

"The back of the bag is one side of the pouch, and the other side is there, in front of it, very cushoning. So there is a pouch inside. For the price, I really like this backpack. It is spacious and yet, quite lightweight."

not convenient

POSTED BY:
Overall rating: 1.0 out of 5

"there is no pouche inside, it's not gonna hold the laptop so it's not working!"