An additional battery pack provides extended power to work and play without worries
POSTED BY:
techbitar
Overall rating:
1.0 out of 5
"I have used this battery for over a year and suddenly it stopped charging with an error message "plugged in, not charging." I followed the advice listed on various support forums including Toshiba's but no luck. I never had such a sudden malfunction of batteries before. The replacement cost is too hefty. So now I have a useless laptop, if portability is the primary definition of a laptop. I have been a satisfied owner of 4 Toshiba laptops over the years. This episode is a disappointment. Maybe it's a manufacturer's defect or maybe it's just my bad luck."
POSTED BY:
Trey
,
Clayton, NC
Overall rating:
5.0 out of 5
"This battery is excellent if you are going on a trip or are going to be away from the plug for more that 3 or 4 hours. I have gotten up to 10 hours before having to charge it up again. LOVE IT!!"
POSTED BY:
tomterrific43
,
penna. usa
Overall rating:
5.0 out of 5
"please type the proper way to get full life of battery according to manufactures recomendation... recharge when drained down or recharge at end of daily use. which is the best way as i read both ways in these reviews"
POSTED BY:
Teenager tested
,
Nashua, NH
Overall rating:
5.0 out of 5
"This battery has lasted 10 months before telling me to change it. Use it 16 hours or more a day. Does get charged when it says its at 10%. Video streaming, Internet use, Texting, Facebook. All typical high demands for a teenager. This battery did come with the computer. If you have the lessor model, use it as a backup. There does come the time when you do finally need a NEW battery. Do the simple checks of other possible battery problems first and then just get a new one."
POSTED BY:
Charlie
,
Pawling, New York
Overall rating:
3.0 out of 5
"This is the first laptop that I have ever owned or used. I like my tower better but I am very happy with this product. I am unsure whether or not to get the 12 cell Li-ion battery. It seems that either it works fine or it fails but even the users who like it are not that enthusiastic about it. I think that I'll wait a while as the battery that came with this unit seems to be performing acceptably."
POSTED BY:
pam
,
Nashua, NH
Overall rating:
4.0 out of 5
"I love this laptop! This is the first of many. Got some time to get used to after using a dinosaur desktop. What a difference! Will always to go this way and give my desktop a proper burial!"
POSTED BY:
toshiba man
Overall rating:
4.0 out of 5
"Battery life may vary considerably from specifications depending on product model, configuration, applications, power management settings and features utilized, as well as the natural performance variations produced by the design of individual components. Published battery life numbers are achieved on select models and configurations tested by Toshiba at the time of publication. See “Detailed Specs” for specific battery measurement test. Recharge time varies depending on usage. Battery may not charge while computer is consuming full power. After a period of time, the battery will lose its ability to perform at maximum capacity and will need to be replaced. This is normal for all batteries. Also if you want more life out of your battery let it die and recharge this is will help, and one more thing read your owners manual. Great battery normally get 6 to 8 hours of use."
POSTED BY:
pearce369
,
Florida
Overall rating:
1.0 out of 5
"I purchased my A660 and as others paid to upgrade to extended battery. I have been using Li-Ion batteries in my R/C aircraft and helicopters since their introduction and have been totally satisfied with life and performance. Li-Ion batteries are not suppose to develop memory but this battery went from over 6 hours useful life to no more than an hour within 6 months of purchase. Battery life started to decrease from the very beginning. Having the previous experience with Li-Ion I made sure to always run it down to less than 10% life before charging as recommended and it had made no difference, life started to decrease from the beginning. I have owned several Toshiba laptops over the years and this battery did not impress me enough to purchase a new one to replace it. I do not think the extra cost, weight and size is worth it."
POSTED BY:
Bishop
,
USA
Overall rating:
1.0 out of 5
"Bought Toshiba Satellite in January, also picked up this 12-cell high capacity battery. I kept for days when I know I will not be likely to plug in to a wall outlet. I just recently started using it a couple of months ago. It worked pretty well for a month roughly 5-6 hours. Then it would barely give me 2-2 1/2 hours of use. There were two bios updates to address battery issues, neither helped. I had to pay UPS fees to return, then instead of UPSing me another they email me a code for a coupon for here. Expected processing time here on this site 1-2 weeks plus normal shipping time. Really? A+, N+, and MCSE certified!"
POSTED BY:
KayakBill
,
near Nashville, TN
Overall rating:
5.0 out of 5
"Work 10-hours as a machinist, take this L655-S5156 to work to play music thru my Bose radio, this battery lets my JAM all nite at work and still ahs a couple of hours charge on it after I get home. Great battery!"