PA3923U-2LC3

Toshiba 14-inch USB Mobile LCD Monitor - Matte Finish

Ultra-portable monitor.

MSRP: $199.99
Shop Online
Toshiba 14-inch USB Mobile LCD Monitor - Matte Finish 4.60 out of 5.0 based on 5 user reviews. Average Customer Rating: 4.60 out of 5.0
Read Reviews (5)  | Write Reviews
Energy Star : Energy Star Logo

Monitors - PA3923U-2LC3 Customer Reviews

Great extra monitor

POSTED BY: , Nashville, TN
Overall rating: 4.0 out of 5

"Simply load the driver and plug it in. No cables to mess with. A touch brighter would be nice but it's not bad for USB only. Wish it had a driver for Ubuntu 12.04"

Great Product

POSTED BY: , Providence, RI
Overall rating: 5.0 out of 5

"Transistioning to this monitor from the larger external monitors with various cords was an easy switch. This monitor is more light weight and very easy to use."

Great solution for laptop sharing

POSTED BY:
Overall rating: 4.0 out of 5

"i love the usb monitor, except for one important factor: not bright enough. I use a usb 3.0 powered port that i hoped would eliminate the need for an optional adaptor for power, but the monitor is stuck at 50%. Having to use an adapter to get 100% brightness is a disappointment, so for now i'll just continue w the lower brightness. Otherwise, ingenious."

Good alternative

POSTED BY: , pittsburgh, PA
Overall rating: 5.0 out of 5

"for those who need a monitor that doesn't use conventional wall power, this is the best technology available on today's market. I hope it becomes a UL listed product soon."

It is a wonderful technology. We enter a new era.

POSTED BY: , Tamilnadu, India
Overall rating: 5.0 out of 5

"It is a wonderful technology. We enter a new era of visual technology. It is a useful device for all in few months. Congrates to the technicians."