Toshiba All-in-one DX735-D3360 Desktop

Toshiba DX735-D3360 All-in-One Desktop (23" Widescreen)

MSRP: $1,199.99
All-in-one DX735-D3360 4.17 out of 5.0 based on 6 user reviews. Average Customer Rating: 4.17 out of 5.0
Read Reviews (6)  | Write Reviews
Accessories for the DX735-D3360 All-in-One Desktop

Accessories
Surge Protectors
Routers
Mice & Keyboards
Scanners & Printers
Monitors
Storage

More DX730 All-in-one Desktops
DX730
Model: MSRP:
DX735-D3330 $999.99
DX735-D3360 $1,199.99

All-in-one DX735-D3360 Desktop Customer Reviews

All in One

POSTED BY: , Chicago, IL
Overall rating: 4.0 out of 5

"So, excited to get this all in one. The computer works fine the screen is great. It's a small thing like the mouse (mice) not work properly."

FAIR COULD HAVE BEEN BETTER

POSTED BY: , FLORIDA
Overall rating: 4.0 out of 5

"FIST REALLY BIG PROBLEM IS - NO HDMI OUT TO SECOND SCREEN. EVEN CHEAP LAPTOPS HAVE THAT OPTION BUILT IN."

Nice, but.....

POSTED BY: , Philippines
Overall rating: 3.0 out of 5

"A nice responsive computer with a good value for money"

THE BEST DESKTOP I HAVE EVER OWNED

POSTED BY: , CT
Overall rating: 5.0 out of 5

"I HAVE ALWAYS OWNED TOSHIBA LAPTOPS AND ALWAYS RATED THEM TO BE THE BEST AND NOW THE ALL-IN-ONE DESKTOP IS BY FAR ONE OF IF NOT THE BEST DESKTOP I HAVE EVER OWNED. THE SPEED WITH THE INTEL I7 PROCESSOR WILL BLOW YOU AWAY. ALSO, MY WIFE IS SO HAPPY NOT TO HAVE THE BULKY PROCESSOR SITTING ON TOP OF OUR DESK ANYMORE. SHE LOVES THE COMPACTNESS OF THE ALL-IN-ONE AND THRILLED WITH THE 23" SCREEN AND BUILT IN SPEAKERS. TOSHIBA, YOU CERTAINLY HAVE OUTDONE YOURSELVES WITH DX735-D3360 All-in-One Desktop. WOULD I RECOMMEND THIS TO A FAMILY MEMBER OR FRIEND? HECK YES AND ALREADY HAVE."

Great All-in-One PC

POSTED BY: , Naperville, IL
Overall rating: 5.0 out of 5

"This is my first All-in-One Desktop, and thus far I am very impressed. I would purchase this exact model for my work as well if I wasn't using three monitors to do my job. At home though, it's perfect. The size is great, and so are the hardware features. There is so much technology packed into something no larger than the average widescreen monitor. I do wish that Windows 7 Professional was an option. I had to pay more for an upgrade disc. Also, it doesn't seem to come with a backup CD. There is a recovery partition, but it won't do me much good in case of a hard-disk failure. Finally, I would ask that Toshiba take it easy with the pre-installed software packages. These are minor inconveniences though. Overall, I am extremely satisfied with this product, and would definitely recommend it to others!"

All-in-one

POSTED BY: , Huntington Beach, CA
Overall rating: 4.0 out of 5

"I bought this all-in-one to replace my laptop. I really appreciate the small footprint and 23-inch screen."

MSRP: Reseller/Retailer pricing may vary. Toshiba is not liable for pricing errors.

More All-in-one Desktops
  • LX810LX810
    LX810
    Perfect for HD entertainment
    Powerful performance
    Elegant, compact footprint
    One-cable set-up
    Preloaded with Windows 8
    Starts at: $699.99
  • LX830LX830
    LX830
    Perfect for HD entertainment
    Built for serious performance
    Optional touch screen
    One-cable set-up
    Preloaded with Windows 8
    Starts at: $799.99

Discount Shown in Shopping Cart

Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.