starting at: $
2 models available
Starting at $999.99
$999.99
POSTED BY:
Deeglo the Glo
,
Chicago, IL
For Model: All-in-one DX735-D3360
Overall rating:
4.0 out of 5
"So, excited to get this all in one. The computer works fine the screen is great. It's a small thing like the mouse (mice) not work properly."
POSTED BY:
iNeedIess
,
Candyland, CA
For Model: All-in-one DX735-D3330
Overall rating:
4.0 out of 5
"I use this for gaming, it's works very well (Unless you're streaming.) So it should perform very well for just browsing the internet, etc. The only thing I disliked was what the keyboard and mouse was made out of. They got greasy very easily, and my fingerprints stick on it. One week into using it, my mouse acted up strange as well, and I had to change it to a wired mouse rather than wireless (Was not due to cursor speed or anything.)"
POSTED BY:
JIM
,
FLORIDA
For Model: All-in-one DX735-D3360
Overall rating:
4.0 out of 5
"FIST REALLY BIG PROBLEM IS - NO HDMI OUT TO SECOND SCREEN. EVEN CHEAP LAPTOPS HAVE THAT OPTION BUILT IN."
POSTED BY:
captain
,
Philippines
For Model: All-in-one DX735-D3360
Overall rating:
3.0 out of 5
"A nice responsive computer with a good value for money"
POSTED BY:
olecoach
,
Dallas, TX
For Model: All-in-one DX735-D3330
Overall rating:
4.0 out of 5
"Really excited about the DX735. Was working extremely well for about 6 weeks. Then suddenly it would not power up. Is presently at a warranty provider for repair. If it comes back and continues to function as it did previously I'll be extremely happy, if not ..."
POSTED BY:
Denny
,
CT
For Model: All-in-one DX735-D3360
Overall rating:
5.0 out of 5
"I HAVE ALWAYS OWNED TOSHIBA LAPTOPS AND ALWAYS RATED THEM TO BE THE BEST AND NOW THE ALL-IN-ONE DESKTOP IS BY FAR ONE OF IF NOT THE BEST DESKTOP I HAVE EVER OWNED. THE SPEED WITH THE INTEL I7 PROCESSOR WILL BLOW YOU AWAY. ALSO, MY WIFE IS SO HAPPY NOT TO HAVE THE BULKY PROCESSOR SITTING ON TOP OF OUR DESK ANYMORE. SHE LOVES THE COMPACTNESS OF THE ALL-IN-ONE AND THRILLED WITH THE 23" SCREEN AND BUILT IN SPEAKERS. TOSHIBA, YOU CERTAINLY HAVE OUTDONE YOURSELVES WITH DX735-D3360 All-in-One Desktop. WOULD I RECOMMEND THIS TO A FAMILY MEMBER OR FRIEND? HECK YES AND ALREADY HAVE."
POSTED BY:
Chris
,
Naperville, IL
For Model: All-in-one DX735-D3360
Overall rating:
5.0 out of 5
"This is my first All-in-One Desktop, and thus far I am very impressed. I would purchase this exact model for my work as well if I wasn't using three monitors to do my job. At home though, it's perfect. The size is great, and so are the hardware features. There is so much technology packed into something no larger than the average widescreen monitor. I do wish that Windows 7 Professional was an option. I had to pay more for an upgrade disc. Also, it doesn't seem to come with a backup CD. There is a recovery partition, but it won't do me much good in case of a hard-disk failure. Finally, I would ask that Toshiba take it easy with the pre-installed software packages. These are minor inconveniences though. Overall, I am extremely satisfied with this product, and would definitely recommend it to others!"
POSTED BY:
YiaYia
,
Huntington Beach, CA
For Model: All-in-one DX735-D3360
Overall rating:
4.0 out of 5
"I bought this all-in-one to replace my laptop. I really appreciate the small footprint and 23-inch screen."