Toshiba All-in-one LX830-ST2G01 Desktop

Toshiba LX830-ST2G01 All-in-One Desktop (23" Widescreen)

MSRP: $1,199.99
All-in-one LX830-ST2G01 4.33 out of 5.0 based on 5 user reviews. Average Customer Rating: 4.33 out of 5.0
Read Reviews (5)  | Write Reviews

All-in-one LX830-ST2G01 Desktop Customer Reviews

Awesome All-In-One

POSTED BY: , Eau Claire, WI
Overall rating: 5.0 out of 5

"It's incredibly easy to setup! Only one wire, plug it in, turn it on, with in 5 minutes you are all setup and ready to go. Seemless and perfect. Plus it's superfast. Highly recommended."

POSTED BY:
Overall rating: 5.0 out of 5

"It has reduced wires by 70% and operates beautifully. The 23" screen is wonderful. I am very pleased with my purchase. It was exceedingly easy to set up."

Excellent computer

POSTED BY: , Fort Lauderdale, Florida
Overall rating: 5.0 out of 5

"Delivery took too long but cant fault the All-in-One once it arrived. Does everything it says, set-up was very easy and quick, wireless keyboard and mouse perfectly adequate. Only used for 2 weeks but yet to find anything negative about the computer."

Very good desktop

POSTED BY: , Roanoke Rapids,NC
Overall rating: 5.0 out of 5

"I recommend this desktop for speed and the screen"

LX830

POSTED BY: , NY
Overall rating: 5.0 out of 5

"My LX830 (I3 processor,8GB RAM, Win7) worked great right out of the box. It was the easiest computer set-up i've ever done. It's fast and seems to work very well overall. The built-in speakers are not as good as my previous JBL Platinum set, but the wireless keyboard and mouse are a plus. I look forward to using the built-in web cam. Would recommend this computer to anyone who wants a desktop for general tasking. Good unit for the price."

MSRP: Reseller/Retailer pricing may vary. Toshiba is not liable for pricing errors.

More All-in-one Desktops
  • LX810LX810
    LX810
    Perfect for HD entertainment
    Powerful performance
    Elegant, compact footprint
    One-cable set-up
    Preloaded with Windows 8
    Starts at: $699.99
  • LX830
    LX830
    Perfect for HD entertainment
    Built for serious performance
    Optional touch screen
    One-cable set-up
    Preloaded with Windows 8
    Starts at: $799.99

Discount Shown in Shopping Cart

Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.