Toshiba All-in-one LX835-D3230 Desktop

Toshiba LX835-D3230 All-in-One Desktop (23" Widescreen)

MSRP: $999.99
All-in-one LX835-D3230 5.00 out of 5.0 based on 1 user reviews. Average Customer Rating: 5.00 out of 5.0
Read Reviews (1) 
This product is no longer available at most retail stores, online retailers, resellers, or ToshibaDirect.com.
We recommend taking a look at other LX830 that are available:
LX830 »

All-in-one LX835-D3230 Desktop Customer Reviews

Slick litte unit

POSTED BY: , So.Cal
Overall rating: 5.0 out of 5

"I looked at all the all-in-one desktops out there before pulling the trigger on the Toshiba. I will say that the Toshiba was not my first choice based on looks, until I saw it in person and it clearly looks better than in photos. I think part of that is due to the angled bottom bezel that gives it a different look in photos. I like the Toshiba, size wise since it puts its 23" screen in a more compact package than the others. Easier to transport when you need to. Just unplug the power cord and fold the back stand/support and that is is. It doesn't take up as much room on a desk, as others with a large bottom base. Performance wise it is really quick with the quad core i7. I do alot of HD video editing, and this unit beats my desktop with an Intel 2 quad core which is around 3 years old. Wish one could change the graphics card in these all-in-ones, yet it still does very well, unless you are a hard core gamer and want the top line of everything.:) The screen really pops with outstanding color and contrast. It is not a matte screen so if you have a window behind you take that into account. I hooked up a Logitech mouse and illuminated keyboard, both wireless of course too improve over the stock keyboard and mouse. So if you want something larger than the big laptops, this unit deserves a look!"

MSRP: Reseller/Retailer pricing may vary. Toshiba is not liable for pricing errors.

More All-in-one Desktops
  • LX810LX810
    LX810
    Perfect for HD entertainment
    Powerful performance
    Elegant, compact footprint
    One-cable set-up
    Preloaded with Windows 8
    Starts at: $699.99
  • LX830
    LX830
    Perfect for HD entertainment
    Built for serious performance
    Optional touch screen
    One-cable set-up
    Preloaded with Windows 8
    Starts at: $749.99

Discount Shown in Shopping Cart

Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.