Toshiba All-in-one LX835-D3250 Desktop

Toshiba LX835-D3250 All-in-One Desktop (23" Widescreen)

MSRP: $1,399.99
All-in-one LX835-D3250 4.50 out of 5.0 based on 2 user reviews. Average Customer Rating: 4.50 out of 5.0
Read Reviews (2)  | Write Reviews

All-in-one LX835-D3250 Desktop Customer Reviews

A Good Computer, But...

POSTED BY: , Pahrump, NV
Overall rating: 4.0 out of 5

"The computer is all that that is advertised and works just fine. However, I was extremely disappointed to discover that it has a single 2Tb HD rather than the dual 1Tb HDs that are advertised. I have always used a second HD to back up my primary but I cannot do it with this computer. Imagine my surprise today when I downloaded the Windows 8 Upgrade Manager and it told me that my touchscreen only includes Windows 7 capability and falls ahort on Windows 8. It also told me that there was no Windows 8 driver for the USB 3.0 hardware and that other components were not compatible. I bought this computer (and a second one) specifically to be ready for Windows 8. I guess that I'm not ready. Although it is a fine computer, I would not purchase it again for the reasons cited above."

best desktop

POSTED BY: , Nashville, TN
Overall rating: 5.0 out of 5

"I BOUGHT THIS DESKTOP AND I WORRIED ABOUT SPEED. BUT IT IS INCREDIBLE. FASTER THAN LAPTOP. AWESOME UTILITIES. I LOVE IT. I FORGET MY LAPTOP. THIS KIND OF DEKTOP THIS PRICE!!! I LOVE IT...!!!!"

MSRP: Reseller/Retailer pricing may vary. Toshiba is not liable for pricing errors.

More All-in-one Desktops
  • LX810LX810
    LX810
    Perfect for HD entertainment
    Powerful performance
    Elegant, compact footprint
    One-cable set-up
    Preloaded with Windows 8
    Starts at: $699.99
  • LX830
    LX830
    Perfect for HD entertainment
    Built for serious performance
    Optional touch screen
    One-cable set-up
    Preloaded with Windows 8
    Starts at: $749.99

Discount Shown in Shopping Cart

Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.