Toshiba All-in-one LX835-D3300 Desktop

Toshiba LX835-D3300 All-in-One Desktop (23" Widescreen)

MSRP: $1,088.99
All-in-one LX835-D3300 4.83 out of 5.0 based on 6 user reviews. Average Customer Rating: 4.83 out of 5.0
Read Reviews (6)  | Write Reviews

All-in-one LX835-D3300 Desktop Customer Reviews

great all in one

POSTED BY: , louisville, ky
Overall rating: 5.0 out of 5

""

all in one is great

POSTED BY: , albuquerque,nm
Overall rating: 5.0 out of 5

"Still in early stages of learning and experimenting but so far, just love it"

New Toshiba computer

POSTED BY: , Venice, Fl
Overall rating: 4.0 out of 5

"Well, I think I love this computer, however, the keypad keys do seem to stick. But I simply hate the Windows 8. Rather than let me use the computer and programs that I want, it is so invasive and wants to control my use -- I bought this computer to use the way I want to -- not be always in conflict with the Windows 8 trying to manipulate me its way. I'm nearly ready to remove it and go back to Windows 7--though I only had XP and loved it. We'll see how it goes. My Emails are always being affected -- difficult to open, not able to delete or send, and I still need to have my Sony Laptop with Windows XP nearby so I can access and send Emails."

Excellent

POSTED BY: , florida
Overall rating: 5.0 out of 5

"This computer is amazing the features are slow for me because I am learning Win 8 and apps. I somehow "messed up" the computer's ability to run properly. Turned the system off and Toshiba corrected the errors automatically and I'm up and running again."

Great product

POSTED BY: , Los Angeles, CA
Overall rating: 5.0 out of 5

"I really like the features -- there are so many."

Excellent Product!

POSTED BY: , San Diego, CA
Overall rating: 5.0 out of 5

"Beautiful screen, very responsive and quick to use. Love it!"

MSRP: Reseller/Retailer pricing may vary. Toshiba is not liable for pricing errors.

More All-in-one Desktops
  • LX810LX810
    LX810
    Perfect for HD entertainment
    Powerful performance
    Elegant, compact footprint
    One-cable set-up
    Preloaded with Windows 8
    Starts at: $699.99
  • LX830
    LX830
    Perfect for HD entertainment
    Built for serious performance
    Optional touch screen
    One-cable set-up
    Preloaded with Windows 8
    Starts at: $749.99

Discount Shown in Shopping Cart

Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.