Toshiba All-in-one LX835-D3340 Desktop

Toshiba LX835-D3340 All-in-One Desktop (23" Widescreen)

  • List Price:
  • $999.99
  • Instant Savings:
  • -$100.00

Total Price:

$899.99

Buy Now
All-in-one LX835-D3340 4.57 out of 5.0 based on 7 user reviews. Average Customer Rating: 4.57 out of 5.0
Read Reviews (7)  | Write Reviews

All-in-one LX835-D3340 Desktop Customer Reviews

Great desk top

POSTED BY: , Halethorpe, MD
Overall rating: 4.0 out of 5

"Wonderful desktop, so much less space needed! Love having it all in one."

Excellent - Except For

POSTED BY: , Florida
Overall rating: 4.0 out of 5

"Performance - Screen resolution - Looks, are all excellent but the small keyboard ruins an otherwise excellent package and I can't say I am a supporter of Windows 8. I definitely do not like pre loading Norton software - Unnecessary complication"

Best all-in-one tried.

POSTED BY: , Lebanon, Oregon
Overall rating: 5.0 out of 5

"I tried several models/brands and found this one to be the best performer. They all have one thing in common and that is they won't turn the screen off or go into sleep mode running Windows 8. I am a long time computer tech and haven't figured this problem out yet. Otherwise, I love the computer."

Great machine!

POSTED BY: , Goldsboro, NC
Overall rating: 5.0 out of 5

"The LX835-D3340 is a great value for the money. On the positive side of the ledger is the machine's fast performance. The display is exceptionally sharp and colors are beautifully rendered. The machine is designed so that the wireless keyboard can be easily moved under the display which frees up desktop space when not in use. The high definition tuner and DVR work flawlessly and is exceptionally easy to use. In the minus column is the noisy, cheap plastic keyboard that is not up to the standard of quality that I have come to expect from Toshiba. I replaced the keyboard with a high quality, quiet keyboard from Logitech. The screen is highly reflective, but this criticism is also true of the other all-in-one machines I evaluated. The screen brightness decreases when viewed at an angle so the unit may need to be moved when watching the high definition television or video. The bottom line--a great machine except for the keyboard, thus my overall 5-star rating and a 4-star rating for Features. I would have no reservations recommending this All-In-One to a friend."

nice

POSTED BY: , warren, mi
Overall rating: 4.0 out of 5

"would like to tilt screen. getting used to windows8 is taking some time."

Great PC.

POSTED BY: , Omaha, E
Overall rating: 5.0 out of 5

"I needed speed and a large display for my "main" computer; the LX835 provides it all. I can split screen without a second display and all applications and synchronizations with other computers, and external devices devices really fly."

desktop toshiba

POSTED BY: , olympia wa
Overall rating: 5.0 out of 5

"very good product, thanks"

MSRP: Reseller/Retailer pricing may vary. Toshiba is not liable for pricing errors.

More All-in-one Desktops
  • LX810LX810
    LX810
    Perfect for HD entertainment
    Powerful performance
    Elegant, compact footprint
    One-cable set-up
    Preloaded with Windows 8
    Starts at: $699.99
  • LX830
    LX830
    Perfect for HD entertainment
    Built for serious performance
    Optional touch screen
    One-cable set-up
    Preloaded with Windows 8
    Starts at: $749.99

Discount Shown in Shopping Cart

Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.