Qosmio® X500

1 model available Starting at $1,299.99 $1,299.99
$1,299.99

Qosmio® X500 — Be the king of all creation

  • Delivers elite mobile performance
  • Built for power gaming, HD entertainment, plus
    creating and editing pictures and video
  • Loaded with premium features

1 model starting at:
$
Choose a model to see detailed specs Shop X500 Series

Intel® Core™ i7 Processor

Customer Reviews for Qosmio® X500

Worst Laptop Ever!

POSTED BY: , Jupiter, FL
For Model: Qosmio X505-Q8100X
Overall rating: 2.0 out of 5

"I have never had a computer with so many problems in the two years I've had this laptop. I've went through 5 adapters, Had to send it back to the manufacturer over 3 times for various reasons and it constantly is over heating. I've replaced the fans many times and that still doesn't help. It's only two years old and I regret ever getting such a computer. I will never get a Toshiba again, this is not worth the money!"

Best computer I ever had!!!

POSTED BY: , Fayetteville, NC
For Model: Qosmio X505-Q8100X
Overall rating: 5.0 out of 5

"Since I wanted to do video editing or anything else that has to deal with media production I needed a really good computer for school. I got this big boy and it is loaded!!! So far it's great, the graphics are excellent and it is fast! Plus it has a native 64-bit system which is awesome! The only downfall for me was the fact that it froze a lot during the first couple of months but after some tedious updating it was all good."

Great Laptop

POSTED BY: , Georgia
For Model: Qosmio X505-Q8100X
Overall rating: 4.0 out of 5

"This is a great laptop with great features! I do wish that the buttons for the volume, play/stop, mute and rewind and fast forward were at the top in the middle area of the laptop because with them being on the left side when typing my hand hits those buttons and it can be annoying."

Great Laptop

POSTED BY: , chicago illinois
For Model: Qosmio X505-Q8100X
Overall rating: 5.0 out of 5

"I am extremely happy with this laptop, It has met and exceeded my expectations. My wife uses it when she works from home and loves it. She hated using our other computer when she worked from home."

Having fun with it!

POSTED BY: , ny
For Model: Qosmio X505-Q8100X
Overall rating: 5.0 out of 5

"This is my 3rd Toshiba laptop and I am not surprised that I love it. Truthfully I purchased it just for the graphics. I am a World of Warcraft player and my other machine just couldn't handle it. I am happy to report that the game runs beautifully on it. I actually cannot believe all of the details that I have been missing. If I had to write something bad about this machine it would be that it is not as portable as my previous laptops. I little too large to quickly pick up and go. And if anyone is wondering what happened to my previous toshiba laptops, well, the both of them are still working. I have handed them down to family members. The oldest one is 8yrs old."

Additional Features available in select models

LED Backlit Keyboard
With the cool-looking keyboard on this laptop you’ll be able to keep typing even with the lights down. It’s great for working on planes or in a quiet corner of your favorite café.
Toshiba Extras
Streamline your fun and personalize how you stay organized with free pre-loaded apps like Toshiba Media Controller and Toshiba ReelTime™.
Full HD TruBrite Display
Why settle? Enjoy full, crystal-clear HD visuals with the broad and brilliant 18.4” diagonal widescreen TruBrite® display on the Qosmio® laptop.
Blu-ray™ Disc Player
Savor rich, razor-sharp movies done up in full 1080p high-def, together with luxurious surround sound as you’ve never heard it before.
Choose a pre-configured Qosmio® X500 »

1 model starting at:
$
Shop X500 Series

More Qosmio Laptops
  • F750F750
    Qosmio® F750
    World’s first glasses-free 3D laptop
    Blends entertainment-focused performance + portability
    Distinctive styling
    The latest in 3D technology innovation
    Easy 2D-to-3D content conversion
    Starts at: $1,299.99
  • X770X770
    Qosmio® X770
    Engineered for elite mobile performance
    Tuned for high-end HD & 3D entertainment
    Superbly styled
    Available Intel® quad-core processors
    Brawny NVIDIA® GeForce graphics
    Starts at: $1,149.99

Computers »

Laptops
Satellite®
Tecra®
Satellite Pro®