Toshiba mini notebook NB205-N310BN Laptop

mini notebook NB205-N310BN

MSRP: $399.99 mini notebook NB205-N310BN 4.60 out of 5.0 based on 73 user reviews. Average Customer Rating: 4.60 out of 5.0
Read Reviews (73) 

This laptop is no longer available at most retail stores, online retailers, resellers, or ToshibaDirect.com.
We recommend taking a look at this similar line of laptops:
mini notebook NB500 Series »
Laptop Accessories
Shop for mini notebook NB205-N310BN accessories at ToshibaDirect.com.
Technical Support
Get support for your mini notebook NB205-N310BN or try our Laptop Forums for additional help.
Intel® Atom Processor
Accessories for the mini notebook NB205-N310BN

Accessories
Carrying Cases
Batteries
AC Adapters
Memory
Docking & Expansion

mini notebook NB205-N310BN Laptop Customer Reviews

" Open with"

POSTED BY: , South australia
Overall rating: 5.0 out of 5

"Everytime i click a program it pops up with "open with" and it is really annoying"

This Netbook Rocks!

POSTED BY: , Tulsa, OK
Overall rating: 5.0 out of 5

"I had an Acer Aspire 1 that I wasn't too happy with because of performance and battery life. After doing some research and reading reviews, I decided I should buy this Toshiba netbook. Am I glad I did! It's so much better than the Aspire! One of my favorite features is the oversized and very usable trackpad. It is the best one I've seen and used on any laptop. The battery life is also outstanding. In fact, that was the final selling point for me. Now that I've got the battery charged and in shape, it lasts me over seven hours! That's with constant use! I don't think anyone can match or boast that. I highly recommend this netbook to anyone looking for one. They won't be disappointed."

Perfect laptop for travel and web!

POSTED BY: , Ajijic, MX
Overall rating: 4.0 out of 5

"I have owned a full-size Toshiba laptop in the past and was pleased with it which prompted me to investigate the small model for travel. I am currently traveling for the year and it is perfect! Speed is not great, but that is of no real consequence because of ease of use and portability. Thanks Toshiba for another good product."

perfect!

POSTED BY: , peabody, ma
Overall rating: 5.0 out of 5

"This has been so much fun. I can take it anywhere I go and its compact enough without being ridiculously small. Keyboard is just the right size."

Great maker of LAPTOPS

POSTED BY: , Alexandria, VA
Overall rating: 5.0 out of 5

"TOSHIBA makes good laptops computers. The NB 205 is my second TOSHIBA laptop. I would not have bought a 2d one if I was not pleased with the first one."

Better Than Average Netbook

POSTED BY: , Bronx, NY
Overall rating: 4.0 out of 5

"Pros: Bluetooth, USB sleep charging port, the brown casing avoids fingerprints that the other netbooks who use the black glossy case. Cons: Poor speakers, eratic touchpad."

Mini Notebook

POSTED BY: , Olympia, WA
Overall rating: 5.0 out of 5

"I just love it. It's small enought to take everywhere. I can take it on vacation and trips. Can access my home and work computer."

Awesome Laptop

POSTED BY: , Costa Rica
Overall rating: 5.0 out of 5

"It's a great machine, it works great, i really like the webcam and mic included, the camera has a really good resolution, i would recomend it to everyone"

Nice

POSTED BY:
Overall rating: 4.0 out of 5

"I'm really enjoying my little laptop. I have a few minor quibbles. It's too bad that the windows 7 starter that I got with it won't even let you change the background screen. That's just mean. Also, it would be great if Toshiba offered better Linux support. I'd love to dual boot into Fedora for coding projects, but no luck so far."

Wonderful Surprise

POSTED BY: , Kansas City, Missouri
Overall rating: 5.0 out of 5

"I knew this would be a good product based on the name. However I was really taken aback by the performance! I am running Windows 7 Ultimate, Office Professional, Visual Studio 8, ...... and they all work very well. A truly exceptional product!"