MSRP†: $419.99
Average Customer Rating:

Read Reviews (15)

Carrying Cases
Batteries
AC Adapters
Memory
Docking & Expansion
POSTED BY:
JingleJingle
,
California
Overall rating:
4.0 out of 5
"Ilove this notebook but it needs a little work. Often it changes screens when typing in info. The windows dont open completely and if theres a submit or enter button at the bottom of a page I'm not able to click on it because of that. And the right and left click buttons are too stiff. You definely need a mouse with this one."
POSTED BY:
Sweet
,
Clinton, IL
Overall rating:
5.0 out of 5
"Bought this for the wife. Was so easy to set up and go."
POSTED BY:
stokcok
,
Oklahoma City
Overall rating:
4.0 out of 5
"I researched the product before I bought it. Several reviewers complained about the sensitivity of the pad and mouse. However, I have not experienced any problems. It is just a matter of training yourself not to place your hand in the wrong place. Since I purchased my net book several friends have purchased one and all have been completely satisfied. Yes, I have recommended the product to others, smile. I only wish a full version of Microsoft Windows 7 had came with the net book."
POSTED BY:
Kris D
,
Mahopac, NY
Overall rating:
4.0 out of 5
"I bought this laptop because I only want to surf the web and check email. The keyboard is the best feature...each key is raised, smilar to an actual keyboard. I am enjoying it so far...it's very small but has lots of power."
POSTED BY:
Luda
,
Brookline, MA
Overall rating:
4.0 out of 5
"I got this notebook just for traveling. I take a lot of photos and I needed to be able to upload my images and backup to additional portable drive without carrying full size laptop. Worked well. Nice Netbook. However speakers could be better."
POSTED BY:
gjanko
,
Sparta NJ
Overall rating:
5.0 out of 5
"I received this NB205-N330BN as a birthday present just over a month ago. I also have a DELL laptop and a Macbook. I've purchased a thin dvd burner and installed Windows 7 Ultimate edition. I have been mostly using it by the TV to surf the web while watching TV. Pros - - Small and light. - Ability to set one USB port to charge phone even while netbook is powered if is a great feature. - Toshiba site provided all of the drivers and proprietary software I needed to upgrade to my new version of Windows and they weren't too hard to find. - Upgrade to Win 7 Ultimate was fairly painless. Cons - - I'd like to be able to set a higher screen resolution. I don't mind the small screen but browsing would be easier if I could see more. Sites like Logitech's Harmony Remote site expect a larger screen and make it more difficult to use the lower resolution display. - Twice I've charged it while off, then unplugged. I turned it on several days later and it said it only had 65% left on the battery. - I wouldn't mind if it was faster. It seems to be about the same speed with the Win 7 Starter and the Win 7 Ult. Maybe more memory would help. It only has 1 GB. I'll have to decide which notebook to take on my next trip. It will be between the Mac and the Toshiba."
POSTED BY:
mz jay
,
chestnut ridge,ny
Overall rating:
4.0 out of 5
"love the laptop weight, style having problems putting pics on screensaver"
POSTED BY:
Dan the Man
,
Germany
Overall rating:
5.0 out of 5
"Extremely user-friendly interface and taskbar. Pointing device is very easy to use. Keyboard is also very comfortable. Exterior of netbook retains a clean, polished look throughout usage. Battery life is easily over 8 hours, unless watching back to back movies. Power cord stays in and does not easily slip out. Sound via headphones is very good quality. Absolutely no problems surfing the internet. Video can be choppy with only the battery(as is normal for low-priced netbooks). The onboard speakers are only good, not great."
POSTED BY:
JJ
Overall rating:
5.0 out of 5
"The Toshiba NB205 is a handy, high-quality, proficient, and easy to use netbook that has unlimited uses. Easy to carry, quick to start up, and runs a great speeds. Easy to maneuver on. Keyboard is very friendly and feels as good as a full sized one. Great product with a great price!"
POSTED BY:
TechFreak
,
Northridge, CA
Overall rating:
4.0 out of 5
"I love how long the battery life is with the 6cell battery. The price fit my budget. The chocolate brown is a classy color. I would love to upgrade my 1gb to a 2gb. There is lots of storage space. The keyboard is amazing. It has enough space for me to not feel so cramped up."