Toshiba mini notebook NB205-N330PK Laptop

mini notebook NB205-N330PK

MSRP: $419.99 mini notebook NB205-N330PK 4.60 out of 5.0 based on 5 user reviews. Average Customer Rating: 4.60 out of 5.0
Read Reviews (5) 

This laptop is no longer available at most retail stores, online retailers, resellers, or ToshibaDirect.com.
We recommend taking a look at this similar line of laptops:
mini notebook NB500 Series »
Laptop Accessories
Shop for mini notebook NB205-N330PK accessories at ToshibaDirect.com.
Technical Support
Get support for your mini notebook NB205-N330PK or try our Laptop Forums for additional help.
Intel® Atom Processor
Accessories for the mini notebook NB205-N330PK

Accessories
Carrying Cases
Batteries
AC Adapters
Memory
Docking & Expansion

mini notebook NB205-N330PK Laptop Customer Reviews

Toshiba does it again...

POSTED BY: , Chicago, IL
Overall rating: 5.0 out of 5

"Once again I'd like to Thank, Toshiba, for another Great computer! Weither you have big fingers or small ones this is espeically easy for all to use. Love the Battery Life, when I need to be out & about for long periods of time I can count it lasting as long as I need it. Over-all another Great buy!"

Nicely executed netbook is average

POSTED BY: , Temecula, CA
Overall rating: 4.0 out of 5

"Well finished netbook is an overall nice package with average features and performance. Windows 7 Starter is a disappointment as is speaker and camera performance. An erratic trackpad spoils what is overall good performance for a small computer."

Perfect size, and still comfortable to use!

POSTED BY: , Cincinnati, OH
Overall rating: 5.0 out of 5

"Love the laptop. The keyboard is full size, can read the screen well, and the machine is solidly built. I highly recommend it to any who may consider purchasing it. Incidentally, it is my 4th Toshiba laptop, and all have been extremely reliable."

Sweet!

POSTED BY: , Indianapolis, IN
Overall rating: 4.0 out of 5

"I love my little pink netbook! It fits right in my purse and is great for travel. I use my Bose earbuds with it to view Neflix videos and it works great! Touch pad could be better.. Called support with a tech question and got fast, excellent help!"

Love it!

POSTED BY: , Houston, TX
Overall rating: 5.0 out of 5

"This little jewel is perfect for what I wanted! The colors on the screen are great, no problem reading anything on the smaller display. Granted you have to scroll down more then on my 17" but that isn't a problem. I also have a 2 year old Toshiba 17" laptop which we drug all over Europe for seven weeks right after I got it, and although it is great for doing all the serious stuff I wanted a smaller (and much lighter) one that I could take pretty much everywhere and this netbook is perfect for me. I did upgrade the Windows 7 Starter to Windows 7 Home Premium. Battery life is 3 times what it is on my 17" which is really handy traveling. The 250 gig hard drive is certainly enough for all my pictures, music, etc. I also ordered the sleeve that Toshiba sells for this netbook since the sleeves that I found at other places wouldn't quite fit due to the battery placement on the back. I have bought 3 laptops through Toshiba Direct and their customer service is great. Very happy customer!"