Toshiba mini notebook NB305-N600 Laptop

mini notebook NB305-N600

MSRP: $349.99
mini notebook NB305-N600 3.54 out of 5.0 based on 55 user reviews. Average Customer Rating: 3.54 out of 5.0
Read Reviews (55) 
This laptop is no longer available at most retail stores, online retailers, resellers, or ToshibaDirect.com.
We recommend taking a look at this similar line of laptops:
Satellite L840 Series »
Laptop Accessories
Shop for mini notebook NB305-N600 accessories at ToshibaDirect.com.
Technical Support
Get support for your mini notebook NB305-N600 or try our Laptop Forums for additional help.
Intel® Atom Processor
Accessories for the mini notebook NB305-N600

Accessories
Carrying Cases
Batteries
AC Adapters
Docking & Expansion

mini notebook NB305-N600 Laptop Customer Reviews

A Great portable office!

POSTED BY: , Mayville, WI
Overall rating: 4.0 out of 5

"The computer is solid -- not cheaply made, and the battery life is excellent! I had an ASUS netbook and it was flimsy and hard to type on. The keyboard on the Toshiba is MUCH better! This is not a gamer computer, but I use it mostly for taking notes, email, etc. when I'm away from the office. I'd recommend it to anyone! The only thing that I would improve is its 2 GB system memory (with upgrade) - it's still a little slower that I would like."

1st Notebook

POSTED BY: , Auburn, IN
Overall rating: 4.0 out of 5

"Simply put I was looking for something small, light weight, etc. to take with me when I traveled. Something that would allow internet and email for the most but able to watch a dvd if that was my desire. I searched and compared diligently and ended up selecting the Toshiba NB305-N600. Overall I have found it to be quite acceptable, however, as is almost always the case nothing is perfect. I was disappointed to find that I could not do a total recovery as I have always been able to do with all previous computers. I don't know about anyone else but probrams are so complicated these days that it is all but inevitable that any computer I own will eventually totally stop functioning. This causes me to desire the "total recovery option" as in return to just like it came out of the box. This came with Windows 7 starter so maybe if I upgrade, for a cost, I will have the total recovery feature that I am used to. One last note, the volume on this notebook is non existent. I don't know if it is just the design or if I have a defective computer. Only time will tell if I figure it out."

Good Laptop

POSTED BY: , Galesburg Il
Overall rating: 4.0 out of 5

"So far so good battery life is great!"

Disappointed

POSTED BY: , Oakland, CA
Overall rating: 1.0 out of 5

"This laptop is slow and oftentimes fails to carry out simple commands. It is particualrly unresponsive on the internet, as compared to other computers I use on the same wireless system. It is so inefficient and slow that I have stopped using the laptop for internet use. In short, this is a poor excuse for a legitimate netbook."

Over heating and bus clock problems

POSTED BY: , Redmond, WA
Overall rating: 1.0 out of 5

"Have had my unit for 3 days now and ready to return. Runs super hot (never under 57C) and yet bus clock sticks at 305MHz (CPU 0.68GHz) (it should be able to step up to 667MHz/1.5GHz). Tried on bundled Win7 Starter as well as fresh Win7 64bit and Fedora 16 64 bit. No difference. Multi Core and Dynamic and Execute Bit enabled in BIOS. Tried everything but couldn't bump WEI CPU Score over 1.7. Needless to say, I'm very disappointed."

You are buying HD protection & a great shell

POSTED BY: , Seattle, WA
Overall rating: 4.0 out of 5

"I've owned the NB305-N600 for 6 mos and I'm pretty happy with it. What you are buying with this netbook is a hard disk 3D sensor, a beautiful hard shell around the computer, and easy access to the hard disk and memory compartments. Otherwise it's the same old boring netbook spec we've seen for years. Having said that, this machine is tough enough to work again and again in Economy Class of a budget airline. If you bump up the memory to 2GB, upgrade Window 7 to Home Premium, and stay away from heavy graphics use, the NB305-N600 has enough power to write email and read PDF documents. Watching streamed video is just about the limit of this machine's capabilities."

Best Mini Ever!

POSTED BY: , Baltimore, MD
Overall rating: 5.0 out of 5

"I love this! It works really great and the battery life is really good. I use this mini for college mostly but I also use it for everyday things as well. The performance works really well."

Best ever!

POSTED BY: , Minneapolis, mn
Overall rating: 5.0 out of 5

"Could not be happier with this lil guy. Sold my I pad and only use the net book. Netflix, you tube and torrents it does it all!"

dependable fast netbook

POSTED BY: , Upper Arlington, OH
Overall rating: 4.0 out of 5

"solid performing netbook. Does well in everyday activities at home, and does quite well for most office use. Found it to perform well in most office duties, except U tube use, and is great for those who travel. Would have been nice to have a D drive partition that was blank included for a needed back up of the original software and registry. Just install windows 7 service pack one AFTER you have done all your other updates ( much better performance). High value and daily performance out of this small package for a good price"

Good For an Average User

POSTED BY: , Northlake, IL
Overall rating: 4.0 out of 5

"Not sure why everybody is complaining about the battery life; it's pretty good to me... This netbook is good for just browsing and checking your e-mail (hence the "netbook"). My parents gave this netbook to me as a preset and I have no problem with it. The only problem is that it's very laggy (maybe too much crapware...) I used to use Windows, but I converted to Linux and it runs smoothly."

MSRP: Reseller/Retailer pricing may vary. Toshiba is not liable for pricing errors.

Discount Shown in Shopping Cart

Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.