Toshiba mini notebook NB505-N500BL Laptop

mini notebook NB505-N500BL

MSRP: $245.99
mini notebook NB505-N500BL 4.27 out of 5.0 based on 248 user reviews. Average Customer Rating: 4.27 out of 5.0
Read Reviews (248) 
This laptop is no longer available at most retail stores, online retailers, resellers, or ToshibaDirect.com.
We recommend taking a look at this similar line of laptops:
Satellite L840 Series »
Laptop Accessories
Shop for mini notebook NB505-N500BL accessories at ToshibaDirect.com.
Technical Support
Get support for your mini notebook NB505-N500BL or try our Laptop Forums for additional help.
Intel® Atom Processor
Accessories for the mini notebook NB505-N500BL

Accessories
Carrying Cases
Batteries
AC Adapters
Docking & Expansion

mini notebook NB505-N500BL Laptop Customer Reviews

Good for price

POSTED BY: , Indiana
Overall rating: 5.0 out of 5

"I don't use this as my primary. I have a beast gaming laptop for that. But for my on the go computer, this thing is tough. Never too warm, never too weak. It stays cool and I can't max it out, and I am HARD on computers. The system keeps it from running too much at once. If you need more ram, it's easy to upgrade. No problems with this one."

good laptop but bad stuff

POSTED BY: , rossville, in
Overall rating: 3.0 out of 5

"i bought this and i like it it is just it will not let me preform a factory reset on it and it is getting me really mad and i cant find out how to do it"

Good Laptop

POSTED BY: , Bradenton, FL
Overall rating: 5.0 out of 5

"I like the color, blue, and the easy gripping of the mini netbook when the screen is closed. The keyboard is very responsive to touch and feels very good. I like the included Toshiba software already installed on the mini netbook. I prefer the 10.1' screen size over laptops with a 15" screen size. This smaller screen and the fact of not having a CD drive makes the weight more favorable to me. I prefer using my Toshiba 320 GB external hard drive more than a CD or flash drive. I want to upgrade the RAM from 1 GB to 2 GB."

Could be better

POSTED BY: , Dayton, OH
Overall rating: 4.0 out of 5

"Overall, I really like my netbook. I love the size and weight as it makes it really easy to carry around. I travel alot and it's a nice size to carry with me. Not as bulky as a full size laptop. However, it would have been even better if the RAM was upgraded. I'm going to upgrade to 2G but it would be even better if I could get to 3G. I don't understand why there is only 1G installed. I would suggest that 2G should be standard. I shouldn't have to invest more money into it immediately after buying it."

Excellent Netbook

POSTED BY: , Albuquerque, NM
Overall rating: 4.0 out of 5

"Reports of the death of the netbook are premature. They are low-glamor, low-profit (so not Marketing's Dream), but rugged and useful. We got the NB505 mainly to be able to log on while traveling, and it's as good as any Windows computer for that. (A Mac would have cost 4x as much!) For this we loaded it up with freeware: Firefox and LibreOffice portable, IrfanView, Paint.net, YC3, Greenshot, MS Security Essentials, etc., which it runs just fine. The NB505 boots reasonably fast, has been 100% stable, and has a great display. The battery life is so good I turned the brightness way up, even on battery. The minor weaknesses are the keyboard and touchpad ergonomics. Though not as bad as some laptops, the keyboard needs "volcano"-shaped keys to better quickly locate your fingers. The touchpad is smallish and lacks easily detectable edges to help with scrolling. Adding black tape solves this. The camera, microphone, and speaker work just fine ... better than expected (if even expected) in for this price range."

Outstanding Netbook!

POSTED BY: , Central Pennsylvania
Overall rating: 5.0 out of 5

"I purchased this netbook for my 12 year son, but quickly discovered how valuable is would also be to me. It's size and features lend it toward many varied tasks...all of which it accomplished. Great Stuff!!!"

Great Package

POSTED BY: , Lynchburg, Va
Overall rating: 5.0 out of 5

"Love it. Great for a toater. Music, videos, pics, and audible books. For the money you can't beat it. Toshiba support is always on the desktop if you need them. Toshiba and windows updates are on top of it for you too. Files from MS Work go right into and from it with no problem. Have a nice desktop and large laptop but seem to stay on this one the most. Just Handy to have I guess."

mini notebook scoop

POSTED BY: , Erie, Pa
Overall rating: 4.0 out of 5

"Not needing a regular size laptop this mini notebook is what I was looking for - just to check out my emails and go online. I'm on a computer all day at work so not really wanting to go on again at home.Ste"

Exactly What I Needed

POSTED BY: , Thousand Oaks, CA
Overall rating: 5.0 out of 5

"This is the perfect machine for what I needed to use for my work. Light weight, long battery life and almost instant on combine to make this an excellent on the road choice."

My Gift , My Laptop

POSTED BY: , Sheboygan,Wisconsin
Overall rating: 5.0 out of 5

"Our friends have this brand for their laptop. They helped my husband , a novice computer user, to surprise me with this laptop. I can't thank them enough. I was surprised that I could quicklly set it up and enjoy its use. I know I will recommend this laptop to others as well. Sharon"

MSRP: Reseller/Retailer pricing may vary. Toshiba is not liable for pricing errors.

Discount Shown in Shopping Cart

Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.