Toshiba mini notebook NB505-N508BL Laptop

mini notebook NB505-N508BL

MSRP: $269.99
mini notebook NB505-N508BL 4.17 out of 5.0 based on 87 user reviews. Average Customer Rating: 4.17 out of 5.0
Read Reviews (87) 
This laptop is no longer available at most retail stores, online retailers, resellers, or ToshibaDirect.com.
We recommend taking a look at this similar line of laptops:
Satellite L840 Series »
Laptop Accessories
Shop for mini notebook NB505-N508BL accessories at ToshibaDirect.com.
Technical Support
Get support for your mini notebook NB505-N508BL or try our Laptop Forums for additional help.
Intel® Atom Processor
This product may be available at a local business reseller.

Find a Reseller

Accessories for the mini notebook NB505-N508BL

Accessories
Carrying Cases
Batteries
AC Adapters
Docking & Expansion

mini notebook NB505-N508BL Laptop Customer Reviews

My Laptop

POSTED BY: , Philadelphia, PA
Overall rating: 5.0 out of 5

"I love my laptop, it is so easy to use. It can fit anywhere. The graphics on the laptop are great."

hellish

POSTED BY: , pierz mn
Overall rating: 1.0 out of 5

"it over all is rreally bad, only the battery life is bad,but better than every thing else"

Very good!

POSTED BY: , NJ
Overall rating: 5.0 out of 5

"Very solid computer, took it on a motorcycle trip from NJ to Alaska 1 month 11,000 miles on a pannier not even a single problem. Worked every day thru wi-fi, handled hundred of pics and video clips. But I will upgrade ram to 2 G."

Absolutely Fabulous!

POSTED BY: , durango, CO
Overall rating: 5.0 out of 5

"This 505 was a birthday gift in Oct. from my husband and I haven't put it down since! It does everything I need it to do except play discs. It fits in my tote or a backpack. I've even dropped it a couple of times but nothing seems to stop it - thank heavens! Wifi is great at hotspots or at home. I mainly wanted it to download and read books but saw no reason to purchase a book reader. This does the books and so much more for roughly the same price. Also, I don't have to hold it to read and can prop it easily to read in bed. I love how easy it is to adjust brightness, FN My husband had a full size Lenova laptop which is cumbersome and heavy. The battery life on his is horrible and he had to replace the battery after a year. Even he is really impressed with the battery life on my 505". My friend bought herself a laptop but when she saw my netbook, she wished she had purchased it instead. Although she also feels the lack of a disc player is problem. The little plastic feet have lost the piece that keeps it from sliding on my lapdesk. We have glued them back in several times and that is the ONLY problem I've ever had."

Excellent Product

POSTED BY: , Philadelphia, PA
Overall rating: 5.0 out of 5

"I've had my NB505 for about a year now and I remain very pleased with it. I'm impressed by the long battery life, keyboard, bright display, relatively light weight, surface texture, and appearance. Startup and shutdown are fast, even with Windows 7 Starter. Wi-Fi is solid. I've added an inexpensive blue-tooth dongle for connection to my smartphone. Although the screen is bright and clear, it is also the most reflective screen I've ever seen. Under bright office lighting or outdoors, the screen is mirror-like, making it somewhat difficult to view."

worst lap top i have ever used

POSTED BY:
Overall rating: 2.0 out of 5

",its slow, it freezes and i do all the skans i can to speed i up, and as i write this reveiw stop working twice, even using word is a disaster."

Welcome to My Office

POSTED BY: , Buffalo, NY
Overall rating: 5.0 out of 5

"My Toshiba NB 505 is the center of my office. It's light enough to take anywhere in my backpack, or even just a bag, and has enough oomph to stream videos, download whatever and work on your office documents. If I had a complaint, it would be that I can upgrade to just 2 gigs of ram. Still, for a netbook, I would be hard pressed to ask for more performance for the price. I hope that Toshiba will still continue to produce netbooks or something similarly portable in the future because they're the best deal on the market. I've had my NB505 for over a year and have never regretted my purchase for a minute."

First and Last

POSTED BY:
Overall rating: 1.0 out of 5

"This is the first Toshiba i have owned and is likely the last. I was first impressed by the small size and battery life thinking it would be the perfect netbook to take to school. after using it for a while it became annoying to use. the speed it way too slow, upgrading the ram helped a bit but not enough. i am usually a multitasker when it comes to computing but with this thing even running a word doc with nothing else seemed to bog it down. browsing websites was extremely slow even when on a good network. the last straw for me was when I got it out of my backpack and its case i found that the screen was cracked. the whole computer looks perfect, undamaged and abused but somehow the screen managed to crack. this is most likely going to be the last Toshiba I will own, not impressed."

An amazing Netbook!

POSTED BY: , Palawan, Phil.
Overall rating: 5.0 out of 5

"I got the netbook from a raffle draw, and the name is not new to me... I can't help myself but to explore it, and i was surprised that it is a lot different from any other laptops, the features, the way it is made, etc... amazing!"

Great netbook

POSTED BY: , Bridgewater, MA
Overall rating: 5.0 out of 5

"This is the second Toshiba netbook I've owned. (Sadly, the first was was fried when I spilled coffee on it.) I owned the first one for two years and this one for a little over a month. The keyboard is responsive and comfortable. The soft, rubbery cover provides a good grip."

MSRP: Reseller/Retailer pricing may vary. Toshiba is not liable for pricing errors.

Discount Shown in Shopping Cart

Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.