Toshiba Portege M780-S7240 Laptop

Portege M780-S7240

MSRP: $1,799.00 Portege M780-S7240 4.00 out of 5.0 based on 6 user reviews. Average Customer Rating: 4.00 out of 5.0
Read Reviews (6) 

This laptop is no longer available at most retail stores, online retailers, resellers, or ToshibaDirect.com.
We recommend taking a look at this similar line of laptops:
Portege R830 Series »
Laptop Accessories
Shop for Portege M780-S7240 accessories at ToshibaDirect.com.
Technical Support
Get support for your Portege M780-S7240 or try our Laptop Forums for additional help.
Intel® Core™ i7 Processor
Accessories for the Portege M780-S7240

Accessories
Carrying Cases
Batteries
AC Adapters
Memory
Docking & Expansion

Portege M780-S7240 Laptop Customer Reviews

Very Flexible and Useable

POSTED BY: , Huntington Beach, CA
Overall rating: 5.0 out of 5

"The laptop while I am still learning the full extent of its capablities is great. It is light and easy to use. It takes full advantage of Toshiba accessories such as docking station. It is the perfect size and weight for business use."

No complaints. Satisfied.

POSTED BY: , Blacksburg, VA
Overall rating: 5.0 out of 5

"I'm a student at Virginia Tech, and was required to get a tablet by the engineering program. I choose the Toshiba over the Fujitsu almost soley to be different from everyone else. So I was kind of going on a risk, but I can definitely say that it wasn't a bad call at all. This laptop does a fantastic job at what it promises. I do ALL my homework on here now, and love the flexibility it gives over normal paper. Everyone needs to know that the touchscreen is not even in the same league as apple products. I have an iTouch, and there's just no comparison. However, once you get used to the screen, it's quite nice to use. So give it some time to get used to. It is NOT multitouch, but that's ok. It's not THAT essential. It works fine without it. Windows 7 is great. There are so many little features that make it brilliant. One of my biggest complaints is that the "rotate" button simply does not work. It's not the end of the world, because there are pretty quick ways to do it through the computer. But this really needs to be fixed by toshiba. Can't really think of anything else. I'm happy. It does what it needs to do. I am glad I made this purchase."

Love this laptop !!

POSTED BY: , Ocala,FL
Overall rating: 5.0 out of 5

"The stylus is amazing ,so easy to use. It is the BEST!"

Why

POSTED BY: , Egypt, Alexandria
Overall rating: 2.0 out of 5

"Theoretically speaking, it is exacltly what iam looking for. Practically, beleieve it or not, it is very slow. Its processor looks as if it is suffering even with a simple applications like ms word. Its 4G RAM is just an illusion. The quality of sound is terrible."

Very disappointed

POSTED BY: , USA
Overall rating: 2.0 out of 5

"I want to return the Portege M780-S7240 to the manufactory as soon as I turn on this new product! (I wish I can!) The resolution and the color of the screen look so dull and dark comparing with my old Toshiba Satellite U305 Series that I brought 3 years ago! Also the size of screen although it said 12'1" but the entire laptop actually is as big as the 13'3" laptop but with a smaller screen!!"

Does everything you'd want it to

POSTED BY:
Overall rating: 5.0 out of 5

"The Portege M780-S7240 is my first tablet. I bought it so I could take notes using the stylus as I begin med school in the fall. I opted to go high-end because it's the only computer I plan on using. I am completely satisfied with the M780. Although I haven't really tested the system with very demanding use, the computer always runs very briskly for normal tasks under 64-vit Win 7. The touchscreen works amazingly well, as does the stylus pen. Switching between the two modes of input is seamless. There is no delay between writing with the stylus pen and seeing what you have written on the screen. The screen itself seems very sturdy and resistant to scratching. The screen is very bright, and usually works just fine outside. It's too bad there is no multitouch support, but I'm not exactly sure what I'm missing without it (I don't think there's very much support for it at the moment). The only real negative about the tablet I'd point out is that at 4.5 pounds it's not the lightest ultraportable I've ever seen. Otherwise it's fantastic. Highly recommended."

MSRP: Reseller/Retailer pricing may vary. Toshiba is not liable for pricing errors.

More Portege Laptops
  • R830R830
    Portégé® R830
    No-compromise mobility
    A showcase of innovations
    Exceptionally thin, light and durable
    Extended battery life rating
    Plays CDs and DVDs
    Starts at: $799.99
  • Z830Z830
    Portégé® Z830
    Extremely light & thin
    Packed with intelligent features
    Faster boot-up time
    Up to 8-hour of battery life rating
    Highly durable
    Starts at: $899.99

Toshiba Product Locator

xhide feature

Reseller/Retailer pricing may vary. Toshiba is not liable for pricing errors.

Computers »

Laptops
Satellite®
Tecra®
Qosmio®
Portégé®
Customizable Laptops
Desktops
All-in-One Desktops
Hard Drives and Storage
Desktop External Drives
Portable External Drives
Accessories
dynadock®
Mobile Monitor
See All Accessories
Need Help Choosing A PC?
Laptop Finder
Computer Research Center

Tablets »

Excite™ Tablet
Thrive™ Tablet
Tablet Accessories
Tablet Finder

Televisions »

Internet Televisions
3D Televisions
LED Televisions
LCD Televisions
TV/DVD Combos
TV Accessories
Need Help Choosing A TV?
TV Finder
TV Research Center

Video & Electronics »

Blu-ray Players
DVD Players
DVD Recorders
Camcorders
Electronics Accessories

Explore Toshiba »

Our History
Contact Us
Social Responsibility
Careers
Ways to Buy
Toshiba Events
Our Commercials
Press Room
Reseller Partners
Public/Private Sector
Connect
Connect with us
Connect with us on Facebook Connect with us on Twitter Connect with us on YouTube