Toshiba Portege R700-S1322 Laptop

Portege R700-S1322

MSRP: $1,299.00
Portege R700-S1322 3.86 out of 5.0 based on 7 user reviews. Average Customer Rating: 3.86 out of 5.0
Read Reviews (7) 
This laptop is no longer available at most retail stores, online retailers, resellers, or ToshibaDirect.com.
We recommend taking a look at this similar line of laptops:
Portege R930 Series »
Laptop Accessories
Shop for Portege R700-S1322 accessories at ToshibaDirect.com.
Technical Support
Get support for your Portege R700-S1322 or try our Laptop Forums for additional help.
Intel® Core™ i5 Processor
This product may be available at a local business reseller.

Find a Reseller

Accessories for the Portege R700-S1322

Accessories
Carrying Cases
Batteries
AC Adapters
Docking & Expansion

Portege R700-S1322 Laptop Customer Reviews

Nice size, light weight

POSTED BY: , Phoenix, AZ
Overall rating: 4.0 out of 5

"This replaced my Sony ultra compact which had a 11" display. This is my first Toshiba and I am very impressed. This has the best keyboard ever. The display is bright and crisp. The CPU is quite fast compared to my previous laptop. The DRAM is expandable for future upgrades. Quality fit and finish are excellent. My complaints: Battery life is poor (a trade for CPU power) The excellent keyboard has no lighting. A bit pricey in a crowded market. Overall a fantastic laptop for business travelers. Hope this helps!"

Great laptop

POSTED BY:
Overall rating: 4.0 out of 5

"Love my Portege so far (3 weeks). I especially like the fingerprint recognition! Exceptions: - face recognition still doesn't work - the space bar is positioned funny;many times Irunwords together because pressingthespace bar with my thumb(s) (the normalway) doesn't work. I''m hoping I canget used to it overtime."

Nice package!

POSTED BY: , Bay Area, Cal
Overall rating: 5.0 out of 5

"This would be my 6th Toshiba, and 4th in the Portege line. Although they've strayed a bit from the incredibly lightweight packaging of the R500, which I also have, the R700 is an excellent ergonomics/performance combination, and is still very lightweight compared to others on the market. Yes, as others have said, the fan does run all the time, but I found that by keeping the laptop cool (ie off of a heat-retaining surface), the fan will run on low most of the time. The i5 processor is powerful, and generates heat that must be dissipated. No complaints about this powerhouse - even the fingerprint reader works!"

No complaints

POSTED BY: , Overland Park, KS
Overall rating: 5.0 out of 5

"I primarily use a computer for email, word processing and spreadsheets. This unit is excellent. It is small, lightweight and fast. The CD reader seems to vibrate, but I have used it only once. So far, no complaints."

Review Portege R700-S1322 Laptop

POSTED BY:
Overall rating: 4.0 out of 5

"Good: - no glossy screen (main reason I chose this product) - light weight (I like it) bad: - battery (with normal performance under 4 hours) - CD slot is "loose" - when picking up the laptop, you press the cover of the CD slot, so it is forced to give way/makes an impulse noise"

Laptop with Big Performance in a Small Pachage !!!

POSTED BY: , Stoddard, WI
Overall rating: 4.0 out of 5

"I boght this laptop for my bookeeper so that she could take it with her in her purse when she goes out of town. She has a pretty big purse. It has windows 7 pro on it and this is the 1st windows 7 in our office. We are still trying to get use to the windows 7, but so far I have been able to resolve most compatibility issues with our older software. Having a bit of a problem getting "outlook" to run properly for email, but this is a windows thing and not anything to do with the laptop. So far we are very pleased with it. It sure came with a lot of good extra features not found on normal laptops."

Fan very noisy

POSTED BY: , Lyndhurst, NJ
Overall rating: 1.0 out of 5

"The machine had a very noisy cooling fan which was on almost all the time. The processor was running at 32-35% (and the fan going on full blast like a hair drier) even when no programs were actively running. Also video memory (and Toshiba programs running in the background) eats up a lot of RAM and you are left with only 1.8 GB of RAM out of total 4GB."

MSRP: Reseller/Retailer pricing may vary. Toshiba is not liable for pricing errors.

More Portege Laptops
  • R930R930
    Portégé® R930
    No-compromise mobility
    Thin & light design
    Packed with the latest technology
    Long battery life rating
    Plays CDs and DVDs
    Starts at: $799.99
  • Z930Z930
    Portégé® Z930
    Extremely thin & light
    All the essential features
    Faster boot-up time
    Long battery life rating
    Highly durable
    Starts at: $799.99

Discount Shown in Shopping Cart

Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.