Toshiba Portege R705-P35 Laptop

Portege R705-P35

MSRP: $899.99
Portege R705-P35 4.46 out of 5.0 based on 89 user reviews. Average Customer Rating: 4.46 out of 5.0
Read Reviews (89) 
This laptop is no longer available at most retail stores, online retailers, resellers, or ToshibaDirect.com.
We recommend taking a look at this similar line of laptops:
Portege R930 Series »
Laptop Accessories
Shop for Portege R705-P35 accessories at ToshibaDirect.com.
Technical Support
Get support for your Portege R705-P35 or try our Laptop Forums for additional help.
Intel® Core™ i3 Processor
Accessories for the Portege R705-P35

Accessories
Carrying Cases
Batteries
AC Adapters
Docking & Expansion

Portege R705-P35 Laptop Customer Reviews

Nice and light

POSTED BY: , Iowa
Overall rating: 5.0 out of 5

"Very nice laptop with nice feel on the keys. Very light weight. Fast start up. Quiet. Battery is decent for its size, but it says it has extended life and that is only for about 6 months of use. It considerably drops after then. Lucky to get 1.5 hr 18 months later."

Needs keyboard backlighting.

POSTED BY: , Wayzata, MN
Overall rating: 5.0 out of 5

"This computer needs keyboard backlighting and a switch to disable the wireless receiver/transmitter, other than that, it's a great laptop."

Great Buy

POSTED BY: , South Bend, IN
Overall rating: 5.0 out of 5

"My professional life requires me to travel 100% of the time and drag my laptop with me; not only through airport, but consistently throughout my day. I was looking for a lightweight laptop that was easy to handle and provided me with the power and tools needed to get the job done. I must say; this laptop did it for me. It's the best. Highly recommended."

Very good laptop,

POSTED BY: , Villgs, Fla.
Overall rating: 4.0 out of 5

"Laptop preforms very well, but disappointed in Battery life..I bought this particular laptop cause of up to 8 hours battery life..NO WAY !!!!!!!!..Full charge and will say abt 4 hours.Better check the manufacturers disclaimer..."

Powerful ultra-portable with great value

POSTED BY: , Toronto, Canada
Overall rating: 4.0 out of 5

"Powerful ultra light laptop which doesn't make me feel like I'm compromising anything that's in the regular sized and much heavier laptops. Would be even better if the battery achieved the 8hr rating, but instead you get the average 3-5 hrs or so depending on use."

Small and efficient

POSTED BY: , CT
Overall rating: 5.0 out of 5

"I had a 6 year old inspiron and I was just getting tired of it being slow and not being compatible with updated software at school (I am a first grade teacher). I just love the lightweight size, quick response and clear screen as well as the longer battery life. I almost bought another Inspiron but then I saw this laptop and I changed my mind. A happy new customer to Toshiba. Very happy with it."

Good Value Laptop

POSTED BY: , Manhattan, KS
Overall rating: 4.0 out of 5

"I bought this laptop chiefly due to it's light weight. It has done well. I have had no problems with any of the software on the computer... I would agree with another review that there is too much software with the computer. I have much better resolution in Internet Explorer using the 'full screen' option. My only complaint is the poor quailty internal speakers (but they are light weight). Also, I agree with one review that the keyboard is noisy when typing. It sounds like my fingernails are too long, just the keys being depressed. On the other hand, you can hear each keystroke."

Best valued laptop

POSTED BY: , Manila, PHL
Overall rating: 5.0 out of 5

"The best ultra-portable laptop in its class! Power packed with great features such as durability, long battery life, above average processing, lightweight, with built-in optical drive, eco-friendly, with pre-installed windows 7 OS, face recognition and 4G WIMAX technology ready...the only thing that needs to be enhanced is the audio HW feature. Definitely a must have..."

Best Laptop I've had

POSTED BY: , Winnipeg,MB,Canada
Overall rating: 5.0 out of 5

"We do a lot of travelling and take our laptops everywhere to keep in touch with folks at home and to write daily reports on our where-abouts. This laptop is the right size and weight for this purpose, without being cramped in keyboard or monitor. We also store pictures of our travels and play games in boring hotel rooms, as well as use Skype to reach our son in China. He is a computer program developer and we always ask his opinion before we buy a new computer, then follow his advice. He has had several Toshiba laptops and swears by them for value for money as well as for what he can do with them. So we bought this one on his advice and are more than happy with it. We also have a Toshiba Satelite and are very happy with it for the same reason - value for money along with everything else."

My first Toshiba

POSTED BY: , Ohio
Overall rating: 5.0 out of 5

"I have been using a Dell Inspiron 8200 I bought new in 2003 prior to going to college. This laptop was excellent and is still in supreme operational condition however it was falling apart - plastic coversing off, screen hinges broken (used string to hold it up attached to the fron the latop... Finally, after much review and waiting for the perfect laptop I settled for the 705-35. Likes: look (brushed metal), lightweight, 4gb RAM, 0.5 terabyte HDD Cons: lacks dedicated graphics, screen resolution and quality is sub par for the advanced user. Toshiba BLOATware. My first experience with Toshiba has been positive. I do not feel tha is necessary that they include so much software with their devies. I just want a laptop that is clean and hasn't been molested yet and a nicely partitioned HDD - windows 50GB, programs (50GB), bulk date (400gb)(music, video, photos). Nice laptop for the average user and the masses. Would like an upgraded screen option! PLEASE! Curious to see how it hold ups in 5 years."

MSRP: Reseller/Retailer pricing may vary. Toshiba is not liable for pricing errors.

More Portege Laptops
  • R930R930
    Portégé® R930
    No-compromise mobility
    Thin & light design
    Packed with the latest technology
    Long battery life rating
    Plays CDs and DVDs
    Starts at: $799.99
  • Z930Z930
    Portégé® Z930
    Extremely thin & light
    All the essential features
    Faster boot-up time
    Long battery life rating
    Highly durable
    Starts at: $799.99

Discount Shown in Shopping Cart

Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.