Toshiba Portege R830-S8332 Laptop

Portege R830-S8332

MSRP: $1,649.00
Portege R830-S8332 4.50 out of 5.0 based on 4 user reviews. Average Customer Rating: 4.50 out of 5.0
Read Reviews (4) 
This laptop is no longer available at most retail stores, online retailers, resellers, or ToshibaDirect.com.
We recommend taking a look at this similar line of laptops:
Portege R930 Series »
Laptop Accessories
Shop for Portege R830-S8332 accessories at ToshibaDirect.com.
Technical Support
Get support for your Portege R830-S8332 or try our Laptop Forums for additional help.
Intel® Core™ i7 Processor
This product may be available at a local business reseller.

Find a Reseller

Accessories for the Portege R830-S8332

Accessories
Carrying Cases
Batteries
AC Adapters
Docking & Expansion

Portege R830-S8332 Laptop Customer Reviews

Excellent performance but...

POSTED BY: , MI
Overall rating: 4.0 out of 5

"The R830-S332 is compact and quick. Between the i7 and the SSD, everything feels very fast. But, know this: if you plan on upgrading the SSD to something larger (the 128GB can quickly become cramped) it won't be as easy as you thought. Toshiba has penny-pinched by employing a proprietary SSD connector. Meaning you'll need to A) scrap the idea, or B) do a tear down all the way to the motherboard in order to swap out the SSD ribbon cable with the wacky connector and replace it with one with a standard SATA connector (part #P000531410, or so I'm told). Doable, if you're tech savvy, but way more work than should be required. Another annoyance: since there is no keyboard volume up/down (only mute,) there is also no on-screen volume meter when you change the volume from your external keyboard. Ok, that's a small thing but annoying since this is such a frequently utilized function. Aside from these things, it's an excellent machine, assuming its durability proves out.."

Better power cord management needed

POSTED BY:
Overall rating: 4.0 out of 5

"Everything on the laptop is great except for the power cord management. Grooves on the brick and fasteners on the brick would make wrapping up the power cord much easier."

Very portable, fast laptop

POSTED BY: , Vanceburg KY
Overall rating: 5.0 out of 5

"My R830-S332 is just what I wanted- it is lightweight and handles all operations with great speed and accuracy. The display is bright and vivid and can be adjusted. However... the fingerprint reader is accurate less than half of the time, and the facial recognition feature doesn't work at all. "Come closer, closer, closer... log in unsuccessul." I don't know about the battery life, but I had to rate it to complete this review."

protege laptop

POSTED BY: , lebo,ks
Overall rating: 5.0 out of 5

"very happy with laptop easy to use and light very fast and made with only options i wanted"

MSRP: Reseller/Retailer pricing may vary. Toshiba is not liable for pricing errors.

More Portege Laptops
  • R930R930
    Portégé® R930
    No-compromise mobility
    Thin & light design
    Packed with the latest technology
    Long battery life rating
    Plays CDs and DVDs
    Starts at: $799.99
  • Z930Z930
    Portégé® Z930
    Extremely thin & light
    All the essential features
    Faster boot-up time
    Long battery life rating
    Highly durable
    Starts at: $799.99

Discount Shown in Shopping Cart

Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.