Toshiba Portege R835-P70 Laptop

Portege R835-P70

MSRP: $845.99
Portege R835-P70 4.21 out of 5.0 based on 23 user reviews. Average Customer Rating: 4.21 out of 5.0
Read Reviews (23) 
This laptop is no longer available at most retail stores, online retailers, resellers, or ToshibaDirect.com.
We recommend taking a look at this similar line of laptops:
Portege R930 Series »
Laptop Accessories
Shop for Portege R835-P70 accessories at ToshibaDirect.com.
Technical Support
Get support for your Portege R835-P70 or try our Laptop Forums for additional help.
Intel® Core™ i5 Processor
Accessories for the Portege R835-P70

Accessories
Carrying Cases
Batteries
AC Adapters
Docking & Expansion

Portege R835-P70 Laptop Customer Reviews

Powerful, light, good battery life

POSTED BY:
Overall rating: 5.0 out of 5

"With the portege I've found everything I've been looking for in a laptop - good performance, long battery life, good looks, once I beefed it up with 8GB RAM it became even faster... and I haven't even installed an SSD yet. Really happy with this machine, I've had it for about 4-5 months now, work on it many hours every day, and it's served me very well. Highly recommended."

Excellent choice

POSTED BY:
Overall rating: 4.0 out of 5

"Overall, I've been very impressed with the R835-P70. Long battery life, lightweight, DVD drive, good selection of ports (in number and types). Drawbacks: the screen has to be set at just the right angle to get the best viewing; the utility of Fn keys (F1, F2, etc.) is not optimal (and can't be re-programmed?). Overall: An excellent value."

Fantastic Laptop

POSTED BY: , Mobile AL
Overall rating: 5.0 out of 5

"Got this laptop to replace my old Toshiba 17" which had served me well but I wanted to do away with some weight. So I shopped around and bought this and it is perfect. Huge HD storage and no problems with the 13.3 screen size. A few problems getting use to the keys but trust me no other laptop out-there has a better layout in this size for someone with large hands. The only thing I would have had different is how the keys are attached to the board. They make a clicking sound and sit off the surface a little so you could get dust under the keys. I keep my laptop clean anyway so that should not be a problem. I am not a gamer so I don't know how this laptop would serve in that area but, for business this computer is sweet. One other thing is to keep in mind a large screen to look at is still the best option at home. The college kids have the eyes to look at the small screen into a long night of paperwork. However, old guys like me need a big screen if the job gets to be over an hour. Still I have already wrote some pretty large documents and it hasn't been to hard on the eyes, especially if I enlarge the paper to 135%. I have used Toshiba for a long time and always found them to back up their products 100%. If you want a super computer and a way to reduce weight this is one to really consider."

Excellent Value

POSTED BY: , Central FL
Overall rating: 4.0 out of 5

"Light weight; long battery life with standard battery; perfect for traveling; Touch pad buttons -- a little clicky"

Great on paper but HDD drive design flawed

POSTED BY: , Denver, CO
Overall rating: 1.0 out of 5

"My HDD has just failed for the second time. I must have had 10 computers in my lifetime and never had the problems this one has given me. It seemed like the perfect fit for my needs - lightweight, fast and reasonably priced. However, it failed after 2 weeks, losing considerable work/set up time. Toshiba replaced the hard drive, which then worked for another 3 months, but now Windows is telling me not to use the computer without replacing the hard drive. I am very frustrated and just cannot recommend this computer to anyone but a Toshiba techie."

nice and light

POSTED BY: , Albany,ny
Overall rating: 4.0 out of 5

"We now have 2 portege laptops (same model). I used my wife's before I bought this one. It's light, stays cool and is fast. Very portable to take to hearings. The sound system could be a litle better and sounds a litle tiny. A key board that lighted up at night would be a nice feature. Overall I like it better than the hp that I had been using."

Hard to beat

POSTED BY: , PA
Overall rating: 4.0 out of 5

"Does everything my desktop can but in a small, portable package. The touchpad was hard for me to get accustomed to so I bought a mini-mouse. Very comfortable to use and the size that I needed."

Excellent value

POSTED BY: , Cambridge, MA
Overall rating: 5.0 out of 5

"This is the best value portable laptop I have seen. It is comparable to a Macbook Air for portability, and a Macbook Pro for performance."

I HATE IT

POSTED BY:
Overall rating: 1.0 out of 5

"... my neighbor recommended it; sorry I purchased it."

PERFECT VALUE

POSTED BY: , Mexico
Overall rating: 4.0 out of 5

"For all the price that you pay, you pretty much are saving if you compare with similar products (in my opinion) Fast processor, good performance, great features (emphasis on the ECO MODE and the utilities pre-installed, and you can change if you want, so no issue at all for those people to tend to customize everything). The only thing that i would ask to change could it be to upgrade to another Graphic Card (Nvidia), and convert a fabulous Laptop in a Monster for gaming!!!!.. (if that's means to pay a little more, it is ok with me, just give the option to updrage dear TOSHIBA Team) Great ITEM!!!"

MSRP: Reseller/Retailer pricing may vary. Toshiba is not liable for pricing errors.

More Portege Laptops
  • R930R930
    Portégé® R930
    No-compromise mobility
    Thin & light design
    Packed with the latest technology
    Long battery life rating
    Plays CDs and DVDs
    Starts at: $779.99
  • Z930Z930
    Portégé® Z930
    Extremely thin & light
    All the essential features
    Faster boot-up time
    Long battery life rating
    Highly durable
    Starts at: $799.99
  • Z10tZ10t
    Portégé® Z10t
    Two in one device
    All the essential ports
    Ultra-responsive performance
    Slim & light design
    Long battery life rating
    Starts at: $1,499.00

Discount Shown in Shopping Cart

Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.