POSTED BY:
Crunchy
,
Portland, OR
Overall rating:
4.0 out of 5
"It's a nice decent workhorse. It does everything well, though no aspect of it's performance will blow your mind. I bumped it up to 8 gigs of RAM straight out of the box because that's a cheap no-brainer. I will say that having the optical drive is a nice touch in a piece this small and light. I'm slightly disappointed that Toshiba touts the magnesium body of this line in some of its literature. There is some magnesium, but there's also quite a bit of plastic. So, don't go thinking that this is hewn out of a solid block of metal or anything. Battery life comes in at a solid 7h45min. So far it does a great job of dispersing heat. It's thin and light and easy to carry around. I'd buy it all over again."
POSTED BY:
LEW
,
Minnesota
Overall rating:
5.0 out of 5
"This laptop has all the "good" stuff, light weight 3lb, cd drive, power save settings at the push of a button, all the necessary ports including 1 USB3. The very best laptop I have ever used, and the battery life is totally awesome. After a full day of use, I still have battery. When they talk of 9 hrs, I believe them."
POSTED BY:
Edward
,
Seattle, WA
Overall rating:
5.0 out of 5
"Great product, I almost bought another product where bad reviews existed. Glad I selected this laptop instead."