Toshiba Portege R835-ST6N01 Laptop

Portege R835-ST6N01

MSRP: $799.99
Portege R835-ST6N01 4.31 out of 5.0 based on 12 user reviews. Average Customer Rating: 4.31 out of 5.0
Read Reviews (12) 
This laptop is no longer available at most retail stores, online retailers, resellers, or ToshibaDirect.com.
We recommend taking a look at this similar line of laptops:
Portege R930 Series »
Laptop Accessories
Shop for Portege R835-ST6N01 accessories at ToshibaDirect.com.
Technical Support
Get support for your Portege R835-ST6N01 or try our Laptop Forums for additional help.
Intel® Core™ i3 Processor
Accessories for the Portege R835-ST6N01

Accessories
Carrying Cases
Batteries
AC Adapters
Docking & Expansion

Portege R835-ST6N01 Laptop Customer Reviews

where is the quality for the price

POSTED BY: , louisiana
Overall rating: 3.0 out of 5

"Although very lightweight the touchpad is clunky and not smooth to use, the screen quality is not as crisp as my three year old Toshiba satelitte and the speakers are tin sounding. This was not an inexpensive computer and since I love my old Toshiba, I thought I would be getting the same or better quality."

Toshiba Laptop

POSTED BY:
Overall rating: 1.0 out of 5

"The laptop doesnt boot up and even reinstalling back to factory settings does not help."

Fast & Light

POSTED BY:
Overall rating: 5.0 out of 5

"This laptop is super light and idea for when with traveling. It is very fast and easy to use. The thing I like best is the lightness and ease that I get with having a full keyboard and screen instead of with a netbook (which I compared and the netbook was both heavier and wider)"

POSTED BY:
Overall rating: 5.0 out of 5

"Love this laptop!! Lightweight, fast, and long battery life. Great price!"

Good Lightweight unit

POSTED BY: , Sacramento, CA
Overall rating: 4.0 out of 5

"Pros: lightweight, CD-ROM, user-upgradable hard drive (SSD) and RAM and battery, HDMI and eSATA output, good webcam, good wifi antenna Cons: no backlit keyboard or keyboard illumination via led, no additional mouse pointer--must use trackpad or external mouse, significant heat buildup, fan noise, loud trackpad buttons The screen resolution could be higher, but it is sufficient"

Good size with DVD SuperMulti

POSTED BY: , Houston, TX
Overall rating: 5.0 out of 5

"Good price with this thin Notebook with DVD SuperMulti."

Best laptop EVER !!!

POSTED BY: , Dallas, Texas
Overall rating: 5.0 out of 5

"I can't say enough great things about this laptop, it's sleek, light weight and has everything that I ever wanted in a laptop. I would highly recommend this laptop to anyone that is looking for one."

I love it

POSTED BY: , Ca
Overall rating: 5.0 out of 5

"I just love my new protege. It is light, stylish, and the price is very reasonable for a very portable laptop. And it comes with cd drive, that rocks too. My friend was jealous when he saw my new protege. The only cons is, I wish the have a prebuilt one with matt screen. Then it will a six star rating!! And I also hope toshiba has a logo like apple or Fujitsu ...."

Great laptop

POSTED BY: , Mableton, GA
Overall rating: 5.0 out of 5

"I'm still adapting to the slightly scrunched in keyboard, but the battery life is nothing short of amazing. Processing speed is great. Really enjoying this new laptop. Weight is fabulous."

Big upgrade from previous laptop

POSTED BY: , Holland, MI
Overall rating: 5.0 out of 5

"Needed a smaller laptop for traveling but still wanted it to be full featured. This machine meets my needs completely for that purpose. Don't think it will ever become my primary machine due to its small size but I didn't expect it to. Meanwhile my spouse is enjoying it too."

MSRP: Reseller/Retailer pricing may vary. Toshiba is not liable for pricing errors.

More Portege Laptops
  • R930R930
    Portégé® R930
    No-compromise mobility
    Thin & light design
    Packed with the latest technology
    Long battery life rating
    Plays CDs and DVDs
    Starts at: $779.99
  • Z930Z930
    Portégé® Z930
    Extremely thin & light
    All the essential features
    Faster boot-up time
    Long battery life rating
    Highly durable
    Starts at: $799.99
  • Z10tZ10t
    Portégé® Z10t
    Two in one device
    All the essential ports
    Ultra-responsive performance
    Slim & light design
    Long battery life rating
    Starts at: $1,499.00

Discount Shown in Shopping Cart

Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.