Toshiba Portege R835-ST6N02 Laptop

Portege R835-ST6N02

MSRP: $899.99
Portege R835-ST6N02 4.44 out of 5.0 based on 14 user reviews. Average Customer Rating: 4.44 out of 5.0
Read Reviews (14)  | Write Reviews
Intel® Core™ i5 Processor
Accessories for the Portege R835-ST6N02

Accessories
Carrying Cases
Batteries
AC Adapters
Docking & Expansion

Portege R835-ST6N02 Laptop Customer Reviews

Great

POSTED BY: , Texas
Overall rating: 5.0 out of 5

"Got this for son's birthday. He really wanted a Ultrabook because of the weight. This laptop is lighter than most of the ultrabooks and it has a lot more memory and bigger hard drive. He loves it says it couldn't be more perfect"

Great Laptop!

POSTED BY: , Berlin, CT
Overall rating: 5.0 out of 5

"I've been using this laptop for a few weeks now and haven't had any problems with it. It is very thin and light so it is easy to carry. It was good battery life and is easy to use. When downloading software it does get a little noisy, but is perfect other than that. Would recommend to everyone!"

review

POSTED BY: , Provo, UT
Overall rating: 3.0 out of 5

"Lightweight, reasonably fast, larger hard drive, long battery life is what I looked for for myself and my twin daughters at college. I was worried about reviews concerning the flimsy screen but bought anyway. One week after I received the new laptop, my daughters came up and showed me their cracked screen cases - same spot on both pcs. A major design flaw that I will probably experience on my new laptop. Not happy. Had trouble with the unit starting after a downloaded "upgrade" from Toshiba. Had to pull the battery to get the system to re-find itself."

touchy touch pad

POSTED BY: , NYC
Overall rating: 4.0 out of 5

"I really like my new laptop but I find the touchpad to be a little finnicky ... skewing wildly depending on where my hand rests. I play a lot of online scrabble and tapping on the scrabble board to change directions almost never works properly. But I love the weight, battery life, speed, so I guess I'll just have to get used to the instability of the touch pad."

Dependable, affordable laptop.

POSTED BY: , McPherson, KS
Overall rating: 5.0 out of 5

"This is my second Toshiba laptop, and I bought it specifically because my last one was so dependable and durable. The last one lasted me almost 5 years, and this new Portege is perfect for all my professional needs. I'll be using it for teaching and connecting with far away friends. So far it has exceeded my expectations! Thank you, Toshiba!"

Awesome package

POSTED BY: , Baltimore, MD
Overall rating: 5.0 out of 5

"I love this laptop. It's light, the battery really lasts (they're not lying abou this), and powerful, but it's NOT for gamers. The video memory is shared with the computer's RAM, and if you have a lot open and start a video-intensive game, you will see a performance drop (why I gave it a 4 for performance). However, if you're like me -- travel a bit, want something to do general computer work, crunch numbers, and occassionaly play a game or watch a movie, it's a great box."

Keyboard

POSTED BY: , Costa Mesa, CA
Overall rating: 4.0 out of 5

"The keys on the keyboard are a little small along with the left and right click buttons."

Pretty good

POSTED BY:
Overall rating: 5.0 out of 5

"I am overall very happy with this computer. It is lightweight, fast, and has an excellent screen. On the downside, the keyboard is not backlit (a moderate negative) and it is a little thicker than advertised because it has feet that can't be removed."

Great laptop

POSTED BY: , San Francisco, CA
Overall rating: 4.0 out of 5

"This laptop has been great so far. Here are my three complaints that should be improved in future models: 1) The keys: I would prefer them to be matte/slightly textured instead of glossy, and slightly larger (I think the keys should run side-by-side together instead of having gaps between them). They're also slightly noisy/clicky. 2) The left and right click buttons are extremely noisy. You don't have to use them much if you use the touchpad for touch-to-click, but I like to use the buttons and they're very "clicky" (you couldn't use them in a library without getting a few glares) 3) The fan: It does make a touch of noise when it's working a little extra hard (not more than other laptops probably) Other than that, it's excellent!"

OK

POSTED BY: , NYC
Overall rating: 4.0 out of 5

"light, fast, nice design, bit noisy at times, display colors are pale compared to my previous toshiba,it seems that it lacks clarity, vibration sensor is annoying and preistalled programs do not run sometimes due to so many security certification requirements etc etc. overall OK. i would recomend it for this price."

MSRP: Reseller/Retailer pricing may vary. Toshiba is not liable for pricing errors.

More Portege Laptops
  • R930R930
    Portégé® R930
    No-compromise mobility
    Thin & light design
    Packed with the latest technology
    Long battery life rating
    Plays CDs and DVDs
    Starts at: $849.99
  • Z930Z930
    Portégé® Z930
    Extremely thin & light
    All the essential features
    Faster boot-up time
    Long battery life rating
    Highly durable
    Starts at: $849.99

Discount Shown in Shopping Cart

Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.