Toshiba Portege Z830-S8302 Laptop

Portege Z830-S8302

MSRP: $1,429.00 Portege Z830-S8302 4.00 out of 5.0 based on 12 user reviews. Average Customer Rating: 4.00 out of 5.0
Read Reviews (12)  | Write Reviews

Available at ToshibaDirect.com
(Usually ships in 1-2 business days)
Add to Cart
Available at business resellers
Intel® Core™ i7 Processor Laptop : 4 Stars Review
Customize your Z830 at ToshibaDirect.com

Customize

Accessories for the Portege Z830-S8302

Accessories
Carrying Cases
AC Adapters
Docking & Expansion

More Portege Z830 Series Laptops
Z830
Model: MSRP:
Z835-P330 $899.99
Z835-P360 $899.99
Z835-ST8305 $899.99
Z835-ST6N02 $999.99
Z835-P372 $1,049.99
Z835-P370 $1,049.99
Z830-S8301 $1,199.00
Z835-ST6N03 $1,199.99
Z830-S8302 $1,429.00

Portege Z830-S8302 Laptop Customer Reviews

Not meeting ultra book standard

POSTED BY: , Cupertino, CA
Overall rating: 2.0 out of 5

"I used Toshiba Dynabook and bought Protégé Z830-S8302. Pros: - Extremely light weight - Excellent form factor - Excellent Battery life Cons: - Poor Power cord design (easily comes out from Laptop) - Noisy Fan - Lower Display resolution (must be same or higher than Apple MACBOOK Air) - Keyboard feeling is not good - First time setup took long time (32bit/64bit selection)"

almost perfect

POSTED BY: , United Arab Emirates
Overall rating: 4.0 out of 5

"I can say its the best,but not perfect,best bcoz it fast,portable,light weight,slim just look like a 13.3 Tablet if closed,unti spills keyboard w/ backlight,BUT not perfect bcoz it got only 6gb and no DVDmulti drive,..as I mark up there the performance is exelent and battery life Rocks,...DID I USE THE SANDWICH TECHNIQUE?:)"

ULTRA TO THE MAX

POSTED BY: , OHIO
Overall rating: 5.0 out of 5

"LIGHTENING FAST, LIGHT WEIGHT AND PORTABLE. GREAT FOR WORK AND PLAY. DID I MENTION THAT IT IS FAST?"

Super Ultrabook

POSTED BY: , Dallas, TX
Overall rating: 5.0 out of 5

"Z 830 is a remarkable machine. It has met or exceeded all of my expectations. Looks great and everyone that has seen it wants one! Have not traveled with it as yet, but expect its continuing performance."

OK

POSTED BY: , Hong kong
Overall rating: 2.0 out of 5

"The PC is better than Ansus, the hard drive is not enough , i need more than 256 g. Hong"

Awesomest Ultrabook but impossible to use!

POSTED BY: , Cambridge, MA
Overall rating: 2.0 out of 5

"It hurts my heart to write this review because I really really love this ultrabook. It is almost perfect in every way except for one tiny but horribly annoying detail which Toshiba totally failed to correct: the fan noise. It is absolutely awful! I simply cannot stand it. It drives me insane. Yes I have the 1.60 BIOS version which ameliorated the problem somewhat! Please tell me Toshiba how could you have overlooked this problem? It really is a shame because everything else is just perfect except for that brain hurting buzz."

WOW !!

POSTED BY: , fairmont wv
Overall rating: 5.0 out of 5

"This is the BEST ultrabook on the market by far i bought the Asus i7 first and had a lot of problems so i thought it might just be that 1 laptop so i took it back and exchanged it 2 more times and they all had WIFI problems i just got the Toshiba and love it like i said THE BEST ULTRABOOK BY FAR . BTW the finger reader and back light keyboard rock"

Portege

POSTED BY: , Green Bay, WI
Overall rating: 4.0 out of 5

"The computer is great for traveling and being mobile. It is very sleek and it does not sacrifice processing power and capabilities for the appearance of the computer. I have had some issues with the HDMI cable plug in while streaming movies from Netflix, it cuts in and out and does not always register with my TVs. That is about the only complaint that I have in regards to the actual computer."

POSTED BY: , San Diego
Overall rating: 5.0 out of 5

"It has perfomred as advertised and the set up as very easy and worked with no problems."

Great Choice

POSTED BY: , Indiana
Overall rating: 5.0 out of 5

"I have waited on my order for a month and it was worth the wait. I have read countless reviews and I will have to say I was concerned about what many have said about fan noise. Either that was a problem with the lower end i3 versions or they were greatly exaggerated. In a silent room, you can barely hear the fan. If there is someone talking in the room or a TV is on three rooms away you will never hear the fan. The only thing I think this little beauty could improve upon is there should be an option for a larger hard drive. I can get by with the 128 but a 256 would be a nice option."

MSRP: Reseller/Retailer pricing may vary. Toshiba is not liable for pricing errors.

More Portege Laptops
  • R830R830
    Portégé® R830
    No-compromise mobility
    A showcase of innovations
    Exceptionally thin, light and durable
    Extended battery life rating
    Plays CDs and DVDs
    Starts at: $799.99
  • Z830
    Portégé® Z830
    Extremely light & thin
    Packed with intelligent features
    Faster boot-up time
    Up to 8-hour of battery life rating
    Highly durable
    Starts at: $899.99