Toshiba Portege Z835-ST6N03 Laptop

Portege Z835-ST6N03

MSRP: $1,199.99
Portege Z835-ST6N03 4.77 out of 5.0 based on 22 user reviews. Average Customer Rating: 4.77 out of 5.0
Read Reviews (22) 
This laptop is no longer available at most retail stores, online retailers, resellers, or ToshibaDirect.com.
We recommend taking a look at this similar line of laptops:
Portege Z930 Series »
Laptop Accessories
Shop for Portege Z835-ST6N03 accessories at ToshibaDirect.com.
Technical Support
Get support for your Portege Z835-ST6N03 or try our Laptop Forums for additional help.
Intel® Core™ i7 Processor
Accessories for the Portege Z835-ST6N03

Accessories
Carrying Cases
AC Adapters
Docking & Expansion

Portege Z835-ST6N03 Laptop Customer Reviews

Great Portable Laptop

POSTED BY: , Arlington, VA
Overall rating: 5.0 out of 5

"I was looking for an upgrade to my previous Toshiba laptop and this ultrabook seemed to be the best choice. I looked as several other manufacturers and elected to stay with Toshiba. This laptop weighs about half my previous 13" model. I find the power more than adequate. I can run all my apps without any slow down. I get between 5 -6 hours of battery life. The backlit keyboard is great when working at night. The fingerprint reader makes logging on very easy. I had no problem registering my fingers and it reads them with no problem. I have not found anything I don't like. You will need to purchase an external optical drive for your DVDs. This is part of making this laptop so portable. I don't use a DVD often, but got one for loading some software and accessing CDs."

Exactly What I needed

POSTED BY: , Manassas, VA
Overall rating: 4.0 out of 5

"Compared to it's competition this laptop has held up pretty well so far, bought it mainly because of it's features which were lacking in other Ultra laptops, only improvements needed are better resolution on the monitor besides that it's a winner, go buy one you won't regret it."

Super lightweight computer

POSTED BY: , Milwaukee
Overall rating: 5.0 out of 5

"Love this computer - use it for business and pleasure. It is extremely lightweight and has a fast processing speed. Couldn't be happier."

Featherweight powerhouse

POSTED BY: , Trumbull CT
Overall rating: 5.0 out of 5

"Shedding pounds does not mean sacrificing performance with this I7 laptop. I am amazed at how much quicker everything is compared to the Satellite I bought just two years ago. One problem: The external DVD drive I purchased failed and wound up corrupting the system and I had to put it in the shop to diagnose and get Windows re-installed. I strongly suggest a fresh installation anyway to get rid of all the Toshiba pre-installed software."

So Convenient and Light

POSTED BY: , Chicago, IL
Overall rating: 5.0 out of 5

"This laptop is great for work and travel. It is very light and approximately the size of a magazine. I like being able to throw it in my handbag when I'm traveling, and having it not be too heavy to carry around. The battery lasts for a good 5 hours so I don't have to bring my charger with me. I had it with me at a conference and several people asked about the model number so they could get the same one!"

POSTED BY: , nyc
Overall rating: 4.0 out of 5

"lightweight, fast, good commute laptop."

Great laptop

POSTED BY: , Knoxville, TN
Overall rating: 5.0 out of 5

"Very light and responsive... quick start ups and shutdowns. Moves between various displays and programs quickly. Better battery life than any other laptop I've used before. I do have a problem with either my palm or left hand unintentionally influencing some keys; which moves the cursor."

Toshiba customer database problem

POSTED BY: , North Palm Beach, FL
Overall rating: 5.0 out of 5

"The Toshiba Portege Z835 ST6N03 HAS JUST ONE PROBLEM which I believe may be merely a fix to the firmware. There is an external VGA connector. WHY is the output is limited to 2048 x 1536? The CPU chip is an i7, and the graphics is Intel HD 3000. I have a DELL 30" display of 2560 x 1600 pixels. THE PORTEGE Z835 ST6N03 FAILS TO DRIVE IT AT ITS FULL RESOLUTION. I don't know how the decision was made, but why stop the VGA output at such a low number when reasonable displays go larger? ----------------------------- I've been a Toshiba customer since 2004 when I bought my first Portege. Something has happened to your customer database and I am no longer allowed to login under my email-for-life address of cshutch@umich.edu. I sure wish you would FIX this problem. Thanks, Chuck"

Better than I imagined!

POSTED BY: , Ft. Worth, TX
Overall rating: 5.0 out of 5

"I have been amazed at how much I am enjoying my new Portege Z835-ST6N03 laptop. I love how light it is as well as the back lit keys for when I am traveling. Battery life has also really impressed me."

POSTED BY: , knoxville tn
Overall rating: 5.0 out of 5

"fast as lightening, light as a feather, probably tougher than it looks to be so thin. like the convenience of the touch pad lock, havent found much to complain about, but it is pricey"

MSRP: Reseller/Retailer pricing may vary. Toshiba is not liable for pricing errors.

More Portege Laptops
  • R930R930
    Portégé® R930
    No-compromise mobility
    Thin & light design
    Packed with the latest technology
    Long battery life rating
    Plays CDs and DVDs
    Starts at: $779.99
  • Z930Z930
    Portégé® Z930
    Extremely thin & light
    All the essential features
    Faster boot-up time
    Long battery life rating
    Highly durable
    Starts at: $799.99
  • Z10tZ10t
    Portégé® Z10t
    Two in one device
    All the essential ports
    Ultra-responsive performance
    Slim & light design
    Long battery life rating
    Starts at: $1,499.00

Discount Shown in Shopping Cart

Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.