Toshiba Qosmio X775-Q7273 Laptop

Qosmio X775-Q7273

MSRP: $1,449.99
Qosmio X775-Q7273 3.50 out of 5.0 based on 2 user reviews. Average Customer Rating: 3.50 out of 5.0
Read Reviews (2) 
This laptop is no longer available at most retail stores, online retailers, resellers, or ToshibaDirect.com.
We recommend taking a look at other Qosmio X770s that are available:
Qosmio X770 Series »
Laptop Accessories
Shop for Qosmio X775-Q7273 accessories at ToshibaDirect.com.
Technical Support
Get support for your Qosmio X775-Q7273 or try our Laptop Forums for additional help.
Intel® Core™ i7 Processor
Accessories for the Qosmio X775-Q7273

Accessories
Carrying Cases
Batteries
AC Adapters
Docking & Expansion

Qosmio X775-Q7273 Laptop Customer Reviews

Disappointment

POSTED BY: , Nantucket, MA
Overall rating: 3.0 out of 5

"I was hoping my new Qosmio would be an improvement over my old Qosmio, but sadly I've been disappointed. Yes it has a better graphics card, yes it has more memory, yes it has a SSD drive and more memory than God, but the battery is absolutely abysmal. I bought my first Qosmio (X505-Q894) in Feb. 2011. It had a 18.4" display and it performed wonderfully. I use my laptops primarily as entertainment centers, as I work overseas a good deal of the time and I like to carry my iTunes movies and music with me. I'm also a gamer, so the X505 provided me with great display and responsiveness when playing on-line. When I loose power (electricity) as you do in some countries, from time to time, the X505 was great. I could play music or videos or a game for at least one hour on the battery, and that wasn't in eco-mode, that was in balanced performance mode. All in all the X505 was a brilliant machine. Unfortunately I can't say the same for the X775. Yes it is more light weight. The X505 weighs in at 10+pound without the power adapter and cords. The X775 does perform well, but it has a 17.4" display, which is not a grand as the 18.4" on the X505. But most of all the battery life is almost nonexistent. When the power goes out I get maybe 15 minutes in balanced mode or 25 minutes in eco-mode. The X775 isn't a bad machine... it's well designed and has high performance components. But it's a desktop replacement that needs to be tied to a power source all the time. Despite it's light weight I would not recommend it for someone who wants to use it as a portable computer, simply because of the performance limitations on its battery life."

Qosmio = big and beautiful powerhouse

POSTED BY: , Indianapolis, IN
Overall rating: 4.0 out of 5

"This system is a beast. That goes without saying. At 6.0 lbs it is not light but is packed with more than most can ask for. The only thing I would change is the ability to have a stripped down version. I am currently loading Windows 7 ultimate and the drivers and software I actually WANT on the machine.... A setup that allowed that on initial configuration would have made this perfect. But, for now I am working on a silent install script to install all required drivers & applications I want. Jon"

MSRP: Reseller/Retailer pricing may vary. Toshiba is not liable for pricing errors.

Discount Shown in Shopping Cart

Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.