Toshiba Qosmio X875-Q7380 Laptop

Qosmio X875-Q7380

MSRP: $1,479.99
Qosmio X875-Q7380 4.20 out of 5.0 based on 20 user reviews. Average Customer Rating: 4.20 out of 5.0
Read Reviews (20)  | Write Reviews
Intel® Core i7 Processor
Customize your X870 at ToshibaDirect.com

Customize

Accessories for the Qosmio X875-Q7380

Accessories
Carrying Cases
Batteries
AC Adapters
Docking & Expansion

More Qosmio X870 Series Laptops
X870
Model: MSRP:
X875-Q7380 $1,479.99
X875-Q7190 $1,379.99
X875-Q7390 $1,849.99
X870-BT3G23 $999.99**

*ToshibaDirect Exclusive. Price includes applicable discounts.

**Customizable laptop. Price shown is for base configuration and includes any applicable discounts. Price may change based on customization.

Qosmio X875-Q7380 Laptop Customer Reviews

Nice for the price

POSTED BY: , Nashville, GA
Overall rating: 4.0 out of 5

"Hate Windows 8 and keyboard does not fit into the laptop very well. Aside from these things it flies and will handle whatever you throw at it."

A Beast at Gaming

POSTED BY:
Overall rating: 5.0 out of 5

"This laptop runs the top high-end PC games. Battlefield 3 run on ultra setting and the PC runs cool! The battery goes down a little bit faster when playing a game."

Powerful but.....

POSTED BY:
Overall rating: 1.0 out of 5

"i have had this laptop for over 2 months, i bought it after having another model in the house BUT this is the biggest disappointment. windows 8 is the Terrible. Before you buy this remember you will find your self downgrading (or considering) to windows 7 i would not recommend it"

Good value for money for the specs offered.

POSTED BY:
Overall rating: 5.0 out of 5

"I'll try to make it easy listing out the pros and cons. Pros : 1. Incredibly fast performance as the specs suggests. It seems like nothing can slow this machine down. 2. Good audio output from the quad speakers. 3. Good build quality, laptop feels quite rugged. 4. Very responsive multi-touch pad. 5. Nice design. Cons : 1. Laptop is quite heavy so it’s strenuous to carry around. After all it is a big 17” 2. Mediocre battery backup. About 2 hours for mixed use (media/browsing). 3. Screen resolution could have been FULL HD. 16:9 is OK but not great. 4. I feel the keyboard could have been better. I like the backlit but the keys themselves are not very comfortable. 5. This maybe a individual concern but this laptop has no BluRay DVD player. I am fine with it since I very rarely use BluRay discs. Overall this is a great laptop and a good value for money. When you use the laptop the sheer performance wafts you over the cons so that should not be a big issue. I have been using this for a couple of months now and I love it! Definitely worthy."

OK, not great

POSTED BY: , California
Overall rating: 4.0 out of 5

"Generally, a good machine. Difficult to see the screen clearly from "off" angles or to see the full screen face on. "Mouse" pad is super sensitive, activating even if I have not touched the pad (just the heat of my hand?)."

Great Laptop!

POSTED BY: , Shanghai, China
Overall rating: 5.0 out of 5

"The laptop in general works perfectly, high quality video resolution, audio and images too; the laptop design is probably one of the best features matching black and red colors perfectly, the only problem I found is that its kind of heavy to carry it and the battery just last 2hrs aprox..."

SO worth the money!!!

POSTED BY: , New Braunfels, TX 78130
Overall rating: 5.0 out of 5

"This laptop is a beast. Granted, I am no heavy gamer, but everything I throw @ my Q7380; it just takes it and laughs @ me. I am so glad I bought this Qosmio over the Asus, or the Dell Alienware. If I had to do it all over. I would make this purchase again, Toshiba really made a winner with this Qosmio!!!"

Great but not excellent...

POSTED BY: , Great Falls, MT
Overall rating: 4.0 out of 5

"This laptop was great! The sound,graphics card,and screen all exceeded my expectations! Well really the computer in whole did. I've seen some people whining about battery life but I have to say this isn't a problem really. Given what this laptop can do. That being said I'd rate it a 8/10 only because of when I opened it and took it out of the box the border around the keys was sticking up. I had to push it in myself. Also the optical drive was faulty(spinning up on its own ever few mins.)so I sent it back to the store for replacement.(not paying this type of money just to have to have a repair job done.) Two other things of note. 1. This laptop does get hot while playing games. Didn't matter if it was an hour or of it was 4 hours. It heats up fast. 2.Win.8...really I'm not a fan however it doesn't slow this one down any! Few hours playing around with it and I felt like a pro. I really see no need to downgrade to 7. All in all I love this laptop."

Just the computer I needed

POSTED BY: , Jersey Shore
Overall rating: 5.0 out of 5

"I work quite heavily with Adobe CS6 programs and the power of the computer and NVidia video card are a necessity. I run an extra 23 inch monitor to help spread out my work flow with no problems - more of a desktop than a laptop so the low life of the battery isn't really an issue unless the power goes out"

Great specs great price

POSTED BY: , Philadelphia, Pa
Overall rating: 4.0 out of 5

"This laptop is super fast, the screen is big, the graphics are awesome. I wish there was a way to personalize it though as the only option is red and black. I also wished it came with Windows 7 as Windows 8 has its quirks but that has nothing to do with the laptop itself. Got this to play all my Sims 3 games and I am thrilled at how this laptop handles it all. I am a loyal Toshiba fan as I had a satellite series for about 4 years and never had any issues and this purchase did not disappoint in any way. If you're looking for a system with these specs under any other brand you WILL be paying ALOT. The battery doesn't last long but I keep mine plugged in most of the time so it doesn't bother me too much. I nicknamed my laptop Dream as it is the laptop I always dreamed about :)"

MSRP: Reseller/Retailer pricing may vary. Toshiba is not liable for pricing errors.

Discount Shown in Shopping Cart

Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.