Total Price:
$1,849.99
| Model: | MSRP: | ||
|---|---|---|---|
|
|||
|
|||
|
|||
|
|||
*ToshibaDirect Exclusive. Price includes applicable discounts.
**Customizable laptop. Price shown is for base configuration and includes any applicable discounts. Price may change based on customization.
POSTED BY:
Fanzie
,
Tempe, AZ
Overall rating:
5.0 out of 5
"I love this laptop. It starts up very quickly. No waiting around lot some, it starts right up. It works very quickly. It didn't take long at all to learn Windows 8. However, I think Windows 8 could have some improvements. I always buy Tishiba Lap Tops I have tried many others but always turn to Toshiba when it is time to buy a new one."
POSTED BY:
Bones
,
Columbus Ga
Overall rating:
5.0 out of 5
"I did my research and this is the the best laptop by far and the only 3d for movies and games and the right price"
POSTED BY:
espinosa181b
Overall rating:
5.0 out of 5
"Great design, excellent peromance, I highly recomend my laptop, except for the battery, why did it last only 1 and half our?"
POSTED BY:
BobS
,
PLano, TX
Overall rating:
4.0 out of 5
"I compared this X875 to several other equally configured laptops, and this model offered twice the features/price as others. Its performance is its trademark, near instantaneous boot. I am up, online, with app-doc's open before my other units have reached the login screen. Extremely satisfied with this unit."
POSTED BY:
xsolo
,
Jamaica & US
Overall rating:
5.0 out of 5
"I have a huge super desktop with two 28" 1920 x 1200 screens that really rocks. But I have presentations to do sometimes for my company and wanted to be able to work from anywhere I might be. So I bought the Qosmio X875-Q7390 WOW!!! Blown away. Not taking any chances I got the fan Cooler Master that goes underneath it. So far have not needed it. The utility that comes on the Big Q that tells what is heating and running well or not, shows that everything is fine. I really like this and the value is unbelievable!"
POSTED BY:
simmsd
,
houston tx
Overall rating:
5.0 out of 5
"I have owned Toshiba laptops in the past, and never had any issues with them...This state of the art Qosmio X875-Q7390 that i recently purchased is ideally suited for viewing 3d bluray movies, as well as streamed video in either HD or SD..I thoroughly enjoy using this product.."
POSTED BY:
cdatlas
,
Little Rock, AR
Overall rating:
5.0 out of 5
"This is the best machine I've ever used, my only complaint is that it came with two HDD rather than one HDD and one SSD...I would rather have an SSD than two HDD, even though both HDDs are 2Tb. Other than that I have zero complaints. It runs everything I've thrown at it and has no problems multitasking."
POSTED BY:
Revelation 7
,
Bear, DE
Overall rating:
3.0 out of 5
"1. Out of the box, unit stuck in sleep mode, had to call factory to get help turning on in Win 8? 2. Disc drive door will not open, clicks but doesn't open unless using my finger nail? 3. My mobile hp-450 printer would not work on USB 3 ports. 4. Only one headset jack, cannot listen to speakers and headset, only one or the other. 5. Speed and performance GREAT."
POSTED BY:
jsmasher
,
LA
Overall rating:
5.0 out of 5
"this computer rocks...heavy but packed with awesome feature...love this unit"
POSTED BY:
devonss
,
Randolph, ma
Overall rating:
5.0 out of 5
"Toshiba powerhouse"