MSRP†: $779.99
Average Customer Rating:

Read Reviews (34)

Carrying Cases
Batteries
AC Adapters
Memory
Docking & Expansion
| Model: | MSRP: |
|---|---|
| A500-ST56EX $849.00 | |
| A500-ST56X7 $879.00 | |
| A500-ST56X4 $999.00 | |
POSTED BY:
smokey
,
Spokane wa.
Overall rating:
3.0 out of 5
"All the functions & features work great except for the keyboard which I replaced. The battery is deader than a door nail."
POSTED BY:
ameen fozi
,
yemen
Overall rating:
5.0 out of 5
"Product wonderful and beautiful and very high performance. Excellent battery lasts so long playback time in the development of high performance. But appeared in the recent problem in the screen stops and operates from receiving the same"
POSTED BY:
Shan
,
Pakistan
Overall rating:
4.0 out of 5
"Overall its a GOOD machine covers maximum features."
POSTED BY:
CIDRtheBITER
,
Phoenix,AZ
Overall rating:
5.0 out of 5
"I have owned the A505 laptop for 4 months now and it has been great. Performance wise It is the fastest laptop I have owned, and boot up times are just a few seconds. The 4 gigabytes of ram along with the Core 3 processor make this thin a beauty in multitasking. One thing I really liked was the hard drive protection software that the laptop came with. It really does a good job on protecting the hard drive from bumps and low tempered teenagers. The screen is just unbelievable, it has a really bright glossy screen that just make all content stand out specially when working with pictures. One option that would have blown me away would have been blue tooth functionality built into the laptop, but for the price I can't really complain. Over all if your looking into purchasing these particular toshiba model or any other toshiba model GO for it! Toshiba makes good quality stuff and they have great product warranty and customer support unlike other manufacturers."
POSTED BY:
Mimi29827
Overall rating:
5.0 out of 5
"When I finally decided I had to get another laptop, I didn't hesitate to look at the Satellites. My last one was a work horse of a machine that wasn't prissy about how it was treated. I was afraid the A505 wouldn't satisfy me, but it's great. I had two complaints with the Satellite I had before: the battery didn't last long enough and it overheated on my lap. The A505's battery lasts longer than any I've seen, and the added bar at the back keeps the air flowing and the heat away from my lap. I can't say enough about this machine. Keep giving the quality, I'll keep buying Toshiba! I wouldn't hesitate a second to recommend it to anyone for small business, school, or home use."
POSTED BY:
toshiba user
,
Battle Ground WA
Overall rating:
5.0 out of 5
"i must say this has been an excellent PC- other them my MAC -- Yes i would pick this one again and also recommend to others. This is fast, fantastic sound in the Harman Kardon speaker system, all others had tinny sounding speakers..."
POSTED BY:
notMyName
,
Canada
Overall rating:
5.0 out of 5
"Two things wrong: The battery life can be a bit variable. One charge, I'll get nearly 7 hours of use out of it. The next it'll be around 3 hours. Second thing is the memory card reader is apparently not available on this model, which kindof ticks me off... it has a slot for it though, so I'll probably get one. Pros: Core i3. I got mine for just under 600, and at that price, the i3 boasts excellent bang for your buck. Wonderfully fast little chip. When it's good with battery life, it's great. There is very little pre-installed software (junk anyway. Toshiba does provide some pretty useful stuff) The keyboard is a nice size, and it feels good to type. I usually hate laptop keyboards but I'm quite happy with this one. Graphics are excellent. Yes, the chip is integrated, but it's one of the best integrated graphics systems available. Takes far less power than discreet cards. Fast turning on and shutting down. I've been using a bogged down XP for the last little while, and this is absolutely wonderful in comparison. Not great, not bad: Speakers + realtek audio manager. The speakers sound GREAT from directly above, but at an angle (the way normal people use a laptop :P) they sound a bit off. The realtek audio manager doesn't allow for much customization. Don't care: Smudges. They come off easily, and only show up when you look for them."
POSTED BY:
Bluebummer
,
Chicago, IL
Overall rating:
5.0 out of 5
"After having the original Satallite for 9 years it started to slow down and couldn't keep up. I knew with a laptop lasting that long I couldn't just replace it with anything it had to be another Satallite. This is the best option out there when I was looking and so it was. It plays my cheap computer games that I love as well as keeps a very fast happy connection to the internet. I am sure this computer will stick with me for as long as my old one did!"
POSTED BY:
Schnoodle
,
Bethel, Ohio
Overall rating:
5.0 out of 5
"This laptop is awesome. Perfect sized screen, hard drive, ram, and processor to meet my needs and exceed them. Yea, the glossy finish with the fingerprints downgrade the ascetics but when it’s clean, it’s a really sharp looking laptop that has impressed everyone. The Harmon/Kardon speakers are pretty awesome too. My HP 17” wide screen was a little too bulky but the 16” screen fits my case well. The extended life battery was a real plus for using it in class and had battery life to spare. The performance is great. Overall, a great laptop for the money I have recommended this laptop to several other people. Good job Toshiba!"
POSTED BY:
Lola
Overall rating:
5.0 out of 5
"Con's The fingerprints; but that really doesnt' bother me, I just wipe them off. The disc drive seems flimsy to me and the disc's seem a little hard to remove. The webcam isn't so great. I tried adjusting it the best I could. Pro's It's faster then anything I've had before. Good price. Long battery life If there is anything about this pc I would change it would be the disc drive and I would like a back lit keyboard. Perhaps next time. -)"