Toshiba Satellite A660-ST5N01 Laptop

Satellite A660-ST5N01

MSRP: $599.00
Satellite A660-ST5N01 4.67 out of 5.0 based on 8 user reviews. Average Customer Rating: 4.67 out of 5.0
Read Reviews (8) 
This laptop is no longer available at most retail stores, online retailers, resellers, or ToshibaDirect.com.
We recommend taking a look at this similar line of laptops:
Satellite P850 Series »
Laptop Accessories
Shop for Satellite A660-ST5N01 accessories at ToshibaDirect.com.
Technical Support
Get support for your Satellite A660-ST5N01 or try our Laptop Forums for additional help.
Intel® Pentium® Processor
Accessories for the Satellite A660-ST5N01

Accessories
Carrying Cases
Batteries
AC Adapters
Docking & Expansion

Satellite A660-ST5N01 Laptop Customer Reviews

Great value

POSTED BY: , California, Missouri
Overall rating: 5.0 out of 5

"The laptop is just what I wanted to purchase for my daughter to use in high school. It is nicely equiped and it not come with pre-loaded junk which was greatly appriciated."

Nice little laptop for the price

POSTED BY: , Washington State
Overall rating: 4.0 out of 5

"I'm really happy with the satellite laptops so far. I've had it a little over a month now and haven't had any issues. It's speedy, can take multiple things running at the same time. I'm an average user in the sense that I mostly use it for the internet and games; I haven't had any issues with the games at all so it must have a good graphics card. It does come with some pre-installed crapware and has things scheduled to run at startup that are unnecessary but as long as you know how to change these things it's no problem. Once I went and uninstalled some of the crapware and stopped a good half a dozen unnecessary things starting when I start it up it's been perfect for me! I definitely notice the thing about the keyboard that I read on other reviews before purchasing; the keys do kind of have to be hit a little harder than usual but I tend to be a hard key hitter anyhow so it hasn't bothered me. Also the battery only lasts a couple of hours unplugged steady use so I tend to have to have it plugged in when I'm using it for a long time... Anyways, there's an average user's opinion for you! It's a perfect laptop for the average computer user. No fancy bells and whistles, just a great working little laptop for internetting and gaming."

Great top

POSTED BY: , Bloomingdale,NY
Overall rating: 5.0 out of 5

"Wow what a piece for the price. I would buy another if I could get the same price, my daughter loves it too."

Very Good Value apart from no Recovery DVD.

POSTED BY: , San Diego
Overall rating: 5.0 out of 5

"Used mostly for Word, Powerpoint, Internet, photo editing, Youtube -- this computer does it all. Great value. Nice looking product with lots of features. Would have preferred Recovery DVDs. Saw error message when making mine. Had to call Toshiba customer service; but nice to be talking to a real person in a minute or two. Very helpful."

POSTED BY: , Huntington Beach, CA
Overall rating: 5.0 out of 5

"Excellent computer, fantastic speakers..fast & reliable!"

2nd Toshiba Laptop

POSTED BY: , Cary, NC
Overall rating: 5.0 out of 5

"This is the second Toshiba we have purchased for home use. Love the ease of set up and the quality of the product."

Great Laptop

POSTED BY: , Walnut, CA
Overall rating: 4.0 out of 5

"Best Price ever! Fast and Great Features."

Excellent laptop

POSTED BY: , Tx
Overall rating: 5.0 out of 5

"Alot of features. Great price"
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
Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.