POSTED BY:
Ababneh
,
Amman, Jordan
Overall rating:
5.0 out of 5
"this laptop is great, I like its amazing style , its better from my previous one which was A135-S4527 Audio is great, the only disadvantge of this laptop is the volume control I prefer the wheel control of the volume not touch keys. I recommend it strongly ."
POSTED BY:
Anna72272
,
Arlington, VA
Overall rating:
5.0 out of 5
"I was really impressed with this laptop compare with the previous model Satellite 305D I have. Much better performance, I really enjoy working with it, great quality of graphics and sound."
POSTED BY:
Clevedan
,
Cleveland, OH
Overall rating:
2.0 out of 5
"My previous laptop was a Toshiba Satellite that I gave to my daughter for college. I loved it. This newer one isn't nearly as good. Although it's a 15.6" screen it is difficult to read anything on the screen. And the battery runs down very quickly. The AC power plug is poorly located right next to the door for the DVDs and gets in the way while using it. The "idiot" lights on the the front panel are positioned so that they are not easily noticed while using the computer and the ones on the keyboard MUST be turned off or you can almost see the battery draining as you work. I liked the old Toshiba better."
POSTED BY:
Kris
,
Kunkletown PA
Overall rating:
3.0 out of 5
"I am impressed with the price and the eco friendly energy conservation style. Although, I am disappointed in the performance of the laptop. If plugged in for a long period of time, laptop appears to make funny noises. Maybe it's overheating, but it comes and goes."
POSTED BY:
theckid
,
Somerset, MA
Overall rating:
4.0 out of 5
"I have worked on beefy laptops, but this one tops the charts in my book. But I think the only things that are missing (because of its price) are a internal bluetooth module and a Gigabit Ethernet. 3 USB ports are good enough for the moderate user, plus USB hubs these days are cheap enough to expand your domain. A slight problem with the USB ports are they are a little tight. I had to force a peripheral in it just to get it in. The graphics card flies with all settings to the max on Halflife 2, WOW, and Bioshock. The touch controls are a nice feature. LCD screen is nice and crisp. The audio is very nice. Harmon Kardon speakers make the bass and tones come into harmony with a grand sound. The Wireless N card is a plus to compensate for the Gigabit-less Ethernet. A blueray drive could have been added to this for more appeal as well. Overall this laptop is very nice, I would definitely recommend it to all my friends."