Toshiba Satellite A665-S5173 Laptop

Satellite A665-S5173

MSRP: $789.99
Satellite A665-S5173 4.38 out of 5.0 based on 46 user reviews. Average Customer Rating: 4.38 out of 5.0
Read Reviews (46) 
This laptop is no longer available at most retail stores, online retailers, resellers, or ToshibaDirect.com.
We recommend taking a look at this similar line of laptops:
Satellite P850 Series »
Laptop Accessories
Shop for Satellite A665-S5173 accessories at ToshibaDirect.com.
Technical Support
Get support for your Satellite A665-S5173 or try our Laptop Forums for additional help.
Intel® Core™ i5 Processor
Accessories for the Satellite A665-S5173

Accessories
Carrying Cases
Batteries
AC Adapters
Docking & Expansion

Satellite A665-S5173 Laptop Customer Reviews

Performance and Features

POSTED BY: , New York, NY
Overall rating: 5.0 out of 5

"This is the best investment I have ever purchased. I was looking to replace my other Toshiba and decided to stay with the brand. Since having this i5 processor, I'm amazed at how fast everything pops up with the click of a button. The sound from the Harman/Kardon speakers are amazing. Since I work long hours on it, the backlit keypad comes in handy also. Thank you Toshiba for making great reliable products."

Poor battery life

POSTED BY: , Murfreesboro, TM
Overall rating: 5.0 out of 5

"Battery lasts less than 3 hours with normal use."

Absoulutely Amazing

POSTED BY:
Overall rating: 5.0 out of 5

"This laptop is absoulutely amazing. This is by far the greatest computer ive been on. Runs flawlessly every time I turn it on, the processors reaction is instant,the full size keyboard is very handy, and list goes on! Best laptop in the A665 series, who knows, maybe in the whole toshiba line up?"

Good Lap Top

POSTED BY: , Torrance, CA
Overall rating: 4.0 out of 5

"This is a good unit, but the battery life is NOT as expected"

Best Laptop Yet

POSTED BY: , Catonsville, MD
Overall rating: 5.0 out of 5

"This is my 3rd Toshiba and it's proven to be the best yet. I purchased it for use in my photography business when I had all but used up the hard drive on my older Toshiba and so far it has performed flawlessly."

My first Toshiba

POSTED BY: , Las Vegas, NV
Overall rating: 4.0 out of 5

"I've had several laptops, but this is my first Toshiba. Overall, I like it quite well. Two areas are troubling -(1) the touch pad isn't very easy to use - sometimes doesn't move at all; (2) the spacebar requires a "heavy touch" to put spaces between words. I especially like the backlit keyboard and the built-in 10-key pad."

Love It

POSTED BY: , Ringgold,Ga.
Overall rating: 5.0 out of 5

"I have owned 5 toshiba laptops,3 HP, 4 Lenovos,3 ASUS and 1 Acer,and this is absolutely the best laptop I have owned,bottom line."

Noisy Sound!

POSTED BY:
Overall rating: 3.0 out of 5

"I just purchased a satelllite A665-5173 and whenever I am listening to music on windows media player and run the toshiba pc heatlh diagnostic monitor will appear a noisy sound coming from the speakers. The same problem appears when a move slightly my laptop with the hdd protection turned on or off it doesnt matter that noise appears!!!"

Ok but could be better

POSTED BY: , dallas, Tx
Overall rating: 3.0 out of 5

"I previous had Toshiba L655 S5157 and had little minor problems so I decided to pay extra to get A665 S5173 and believe me its worth since it was on sale. The main issue is the speakers noise clicking, this occurs when I move the laptop around or bump it. Make sure you check your laptop good because once you buy it that’s it."

Laptop

POSTED BY: , Taft, Ca.
Overall rating: 5.0 out of 5

"It works quickly. Has plenty of memory for most situations. Do have a problem with Internet Explorer, but the store loaded Firefox, so am fine. Lighted keyboard is wonderful. I use skype and the picture and sound is great. the Dolby Advanced Audio is the best. I have to turn it down. This laptop replaced my 12 year old HP tower."
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
Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.