Toshiba Satellite A665-S5179 Laptop

Satellite A665-S5179

MSRP: $849.99
Satellite A665-S5179 4.41 out of 5.0 based on 26 user reviews. Average Customer Rating: 4.41 out of 5.0
Read Reviews (26) 
This laptop is no longer available at most retail stores, online retailers, resellers, or ToshibaDirect.com.
We recommend taking a look at this similar line of laptops:
Satellite P850 Series »
Laptop Accessories
Shop for Satellite A665-S5179 accessories at ToshibaDirect.com.
Technical Support
Get support for your Satellite A665-S5179 or try our Laptop Forums for additional help.
Intel® Core™ i5 Processor
Accessories for the Satellite A665-S5179

Accessories
Carrying Cases
Batteries
AC Adapters
Docking & Expansion

Satellite A665-S5179 Laptop Customer Reviews

Perfect Laptop For Me

POSTED BY: , South Padre Island, TX
Overall rating: 5.0 out of 5

"I've been very impressed with this laptop. I've had other High end laptops for professional application and the Toshiba is pleasantly impressive! It can handle an unusual amount of work load and applications. I would recommend this laptop, highly. You Can Not Beat The Price!"

EXCELLENT PC

POSTED BY: , Trujillo Alto, PR
Overall rating: 5.0 out of 5

"this laptop is excellent for the price. without a doubt the best laptop i've ever had."

Solid with a few bugs

POSTED BY: , Virginia
Overall rating: 4.0 out of 5

"Laptop was an upgrade from my last Toshiba so the high resolution screen was nice and the keyboard lighting was nice as well. When I close the laptop and open it back up the screen is often black so I have to put it to sleep and the turn it back on which was very annoying at first but I got used to it now. There was a feature with the mouse where you would be using the cursor and it would unexpectedly zoom in or out, but that can be changed under the mouse options. For some reason this laptop would exit out of my Java application while playing pogo games frequently too, maybe it was the internet explorer. Besides those problems this laptop is nice, I was worried that perhaps the two clickers might get stuck but no problems so far half a year in. Excellent memory storage on here and it runs pretty fast."

Has everything I wanted

POSTED BY: , Littleton, CO
Overall rating: 5.0 out of 5

"This is a feature-rich laptop. Our other laptop is at least 10 years old, so when we got this one we were blown away. It has all the features we needed, plus a Bluray player and an HDMI outlet. Besides using it on the go, we use it to stream Netflix movies to our HDTV and the quality is terrific, much better than the Bluray player in our entertainment center. Other reviews have mentioned that the battery life is poor, but so far we haven't needed to use it more than a couple of hours in areas where we coudln't plug it in."

Best laptop I've had

POSTED BY: , Pasco, WA
Overall rating: 5.0 out of 5

"I have only owned one particular brand computer and decided to branch out and try a 'new' brand this time. I must say I'm not at all sorry I did. This Toshiba Satellite far exceeded my expectations in performance and ease of use."

Works great

POSTED BY: , Fontana, Ca.
Overall rating: 5.0 out of 5

"all futures work great upgreaded an ease have not even need tech suport yet."

Outstanding Value!

POSTED BY: , Northwood, OH
Overall rating: 5.0 out of 5

"This unit offers all of the features that are important to me for a very reasonable price. It's quick, the keyboard is easy to navigate and the image is very sharp. I'm very well pleased!"

Pretty Good...

POSTED BY: , Chicago, Illinois
Overall rating: 4.0 out of 5

"This is an exceptionally great laptop that will do anything for my programming needs. The i5 processor is a dream for the exception that it heats up very quickly. The laptop itself, due to the fast processor, has a low battery life, and if that could improve, it would increase performance tenfold. It is a little bit thick and heavy, but with the great features such as the backlit screen and blu-ray player this latop is definitely worth it. Good job Toshiba!"

Great Features and Performance

POSTED BY: , Tucson, AZ
Overall rating: 5.0 out of 5

"The laptop performs tremendously. There was a complaint from one user about the buzzing sound from the speakers when the unit is moved. This is due to the HDD protection. You can turn it off and the sound won't happen when moving the laptop. Wish it had bluetooth, but happy with HDMI, BluRay, backlit keyboard,built in camera, and audio quality."

Good machine

POSTED BY: , morristown, tn
Overall rating: 5.0 out of 5

"I really like this laptop. I especially like the lighted keyboard since many times I operate in diminished light. The keyboard is comfortable and the keypad is great on this size laptop. I have to praise the weight of this computer. I have owned several other brands such as D... and H. and G. and this computer is lighter for its size than the others. It has great speakers. I think I like it better than any of the other brands that I have used."
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
    Starts at: $870.99
  • L840L840
    Satellite® L840
    Great for everyday computing
    Easy to carry design
    Fashionable and affordable
    Great for enjoying multimedia
    Preloaded with Windows8
    Starts at: $449.99
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
    Starts at: $779.99
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
    Starts at: $524.99
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
    Starts at: $486.99
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
    Starts at: $679.99
  • S870S870
    Satellite® S870
    Great desktop replacement
    Big screen viewing
    Premium speakers
    Entertainment-focused features
    Preloaded with Windows 8
    Starts at: $524.99

Discount Shown in Shopping Cart

Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.