POSTED BY:
Graphicperformance
Overall rating:
3.0 out of 5
"Overall a pretty good computer. It works nice for my multitasking and can have several programs up with no problem. Good features and never had problem with performance unless it was anything needing the graphic card to work I was looking for a computer witch had overall good standards on everything and after looking throu several shops this was what i was reccomended by most. My question would be, why would you have so many awsome components in a computer with a graphic card like this? It basicly kills half of the computer. I can basicly play any game that is currently produced if i could upgrade my graphics (witch is not possible) but because of the current standar of my graphics (Intel (HD) Graphics) I cannot play basic video games even. Im verry disapointed that i now have to sell my Toshiba to buy a new even bether computer. Not only do i lose huge amount of money but it also lose alot of time. I think this was a deceiving computer that looks great on the statistic but when you finaly have it preforming it dosent measure up.. If you want to put one bad component in the computer to pull the price down, make sure its replaceable..."
POSTED BY:
zane
Overall rating:
5.0 out of 5
"First off, this is my 4th Toshiba laptop. i will ONLY buy Toshiba laptops. After the first one 5 years ago, i have learned that Toshiba makes horrible hard drives. So the very first thing ive done is replaced those. This time, i put a SSD in and the laptop is super crazy fast. What Id like to see done on future laptops is the 2nd internal HDD bay activated. Since the cost of SSD is still relatively high for the size, there needs to be a way to hold additional storage that doesnt involve carrying around an external drive. Other than that, this laptop is fantastic, just like i would expect from Toshiba"
POSTED BY:
TLouis
,
Cgicago, Il.
Overall rating:
2.0 out of 5
"Laptop started off good, had everything I wanted. First problem was with the Blue Ray not playing certain movies. The support staff gave me solutions none of which worked. I specifically looked for a laptop with blue ray and I am now going to have to mail it back and wait for weeks . This has not been a good experience and if I could get my money back I would but I am now stuck."
POSTED BY:
Awi
,
Asunción, Paraguay
Overall rating:
5.0 out of 5
"This is my first Toshiba, and I'm impressed. The speed of the i7 quad core is awesome. Extended keyboard is extreamly comfortable. Multitouch pad gives you extra funcionalities. It's perfect for my need, I do computer programming and works like a charm for my environment. I don't do games neither heavy graphic intensive applications, so on board video is more than enough for me. USB 3.0/eSATA port is ultra fast, I bought also a Seagate usb 3.0 external disc, I get peaks of 100MB/s and average of 70MB/s copying big files. Definitively I would recommend this laptop. Looks also is really nice. I can't believe I paid less than 1000 USD for these machine. Very happy customer over here :)"
POSTED BY:
godfather
,
India, Del
Overall rating:
4.0 out of 5
"it is amazing laptop with an really goood look and mind boggling sound clarity and loudness a worth buy"