POSTED BY:
goodcookin
,
Phoenix, AZ
Overall rating:
5.0 out of 5
"This is my third Toshiba Satellite over the years and I cannot be happier. It is a wonderful labptop as I expected. I am thoroughly convinced that the Toshiba Satellite series is fantastic and will continue to buy them."
POSTED BY:
None
Overall rating:
4.0 out of 5
"This is my 3rd Toshiba over the past several years. Overall they are excellent with the only drawback being the battery."
POSTED BY:
Maxdad
Overall rating:
4.0 out of 5
"I love this machine. Very fast processing, always able to handle more. I bought mine with 4GB RAM and changed to 8GB- need the upgrade to make up for very slow hard drive. System takes ridiculous amount of time to cold boot then login. Hibernate/sleep makes startup better."
POSTED BY:
virtuelady
,
San Diego
Overall rating:
3.0 out of 5
"Great machine but two major problems. Impossible space bar that did not space half the time; real problem for production typing and required unusual force, so much so that it caused pain in my thumb. The volume control required several touches to increase volumn. So sorry for these two matters as it was a lot of computer for the money. So sorry, but very disappointed."