Toshiba Satellite A665-S5187X Laptop

Satellite A665-S5187X

MSRP: $879.99
Satellite A665-S5187X 4.25 out of 5.0 based on 4 user reviews. Average Customer Rating: 4.25 out of 5.0
Read Reviews (4) 
This laptop is no longer available at most retail stores, online retailers, resellers, or ToshibaDirect.com.
We recommend taking a look at this similar line of laptops:
Satellite P850 Series »
Laptop Accessories
Shop for Satellite A665-S5187X accessories at ToshibaDirect.com.
Technical Support
Get support for your Satellite A665-S5187X or try our Laptop Forums for additional help.
Intel® Core™ i7 Processor
Accessories for the Satellite A665-S5187X

Accessories
Carrying Cases
Batteries
AC Adapters
Docking & Expansion

Satellite A665-S5187X Laptop Customer Reviews

Excellent Laptop

POSTED BY: , Atlanta, GA
Overall rating: 5.0 out of 5

"I've been using the laptop for about 3 months now. I really like it. The quad core processor is more than enough for any task. I travel weekly and wanted an HDMI port for watching Slingbox on the hotel TV so this was a must. The battery life is pretty good about 3.5 hrs. The webcam was fine for Skype. It has everything 99.9% of the general population will ever use. Great value for the price. This is my 2nd Toshiba laptop. i would recommend it."

Excellent Laptop

POSTED BY: , Irving, Texas
Overall rating: 3.0 out of 5

"Laptop is a very fine work tool. The Core i7 makes a big difference. I wish it had a firewire connection."

I love this computer!

POSTED BY: , Lexington, Kentucky
Overall rating: 5.0 out of 5

"I purchased this computer about one month ago. It is smooth to operate and the graphics are so much better. I feel comfortable using this computer and do not regret the purchase. The speed of the computer is really fast and the high definition screen is great for watching television if you have the connector and movies through the DVD player in the computer. If anyone is thinking about this model, I say get it."

Good For The Price

POSTED BY: , Allen, TX
Overall rating: 4.0 out of 5

"I have been using this laptop for the past week or so. Believe it or not, it is my fifth laptop in 4 days. I have another Toshiba laptop as well and I got the performance that I was expecting from this one as well. This laptop is fast. The best thing about it to me is the sound. The speakers are great, display is bright and the computer is lightweight. The noticeable flaws I found are the webcam is terrible, judging by the price, the laptop only comes with a standard DVD/CD Burner where other manufacturers provide Blue-Ray Drive for lesser priced laptops. Another disadvantage was the lack of a Bluetooth adapter. I was expecting it from an expensive laptop such as this. Overall, keeping the flaws aside, I love this laptop so far."
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
Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.