Toshiba Satellite A665-S6094 Laptop

Satellite A665-S6094

MSRP: $1,026.99
Satellite A665-S6094 3.98 out of 5.0 based on 44 user reviews. Average Customer Rating: 3.98 out of 5.0
Read Reviews (44) 
This laptop is no longer available at most retail stores, online retailers, resellers, or ToshibaDirect.com.
We recommend taking a look at this similar line of laptops:
Satellite P850 Series »
Laptop Accessories
Shop for Satellite A665-S6094 accessories at ToshibaDirect.com.
Technical Support
Get support for your Satellite A665-S6094 or try our Laptop Forums for additional help.
Intel® Core™ i7 Processor
Accessories for the Satellite A665-S6094

Accessories
Carrying Cases
Batteries
AC Adapters
Docking & Expansion

Satellite A665-S6094 Laptop Customer Reviews

Slow boot up, hibernation failures A665-S6094

POSTED BY: , NJ
Overall rating: 2.0 out of 5

"I bought my second Toshiba laptop after 4 years of great service from my first, but I am sorry I did. This machine is terrible for an I7 CPU! It boots slow, constantly crashes from hibernation mode and the touchpad is always switing to scroll mode, I assume based on some design flaw in the outer casing. I was hoping time and care would root out the issues but I suspect I will give this to my daughter for a Facebook machine and buy the Lenova I should have."

Average

POSTED BY: , AUSTRALIA
Overall rating: 3.0 out of 5

"Laptop is very plastic and screen back flexes, hardrive collapsed in first week of use, not very happy, not a nice smooth machine to operate"

Not what I expected from Toshiba.

POSTED BY: , Portland, OR
Overall rating: 2.0 out of 5

"So I got this expecting a quality product from a company I have always relied upon. To my dismay after 3-4 months now I have nothing but 45 minute battery life unless I shut all the little extras off. I have a video card that cant a simple game like Hellgate on lowest setting and still over heat the video card within 15 minutes. Lastly the keyboard only works sometimes, If I press the A, S, or Spacebar button it only works half the time. I like the speed of the computer and streamlined look and feel. I also like the software bundle, but I really should have taken this back after the first week. Not really happy I spent a lot on this laptop, but hey I got it for almost 400 hundred dollars cheaper than they are selling it for on there website."

3 months out and works fine

POSTED BY: , Buffalo, NY
Overall rating: 4.0 out of 5

"I've had this for 3 months now and the laptop is serving me well. Once I took most of the bloatware out this laptop works great for what I need. Replaced another toshiba that had a screen light problem. I repaired that one and gave it to my daughter. I always buy Toshiba as they seem to perform better than any others I tried before. The only problem I've had is that internet explorer has some kind of glitch that intermittently shuts the browser down. It usually restarts itself but this is a pain if I'm gaming. I'm sure eventually an update will cure this problem. The keyboard is great since I now have a num pad to work with. This makes things simpler for me when working with accounting program. Overall I'm happy with the laptop."

One Big Goodness in Many Badness

POSTED BY: , Indonesia
Overall rating: 2.0 out of 5

"Recent Toshiba Laptops' quality are definitely worse than the older ones. What a disappointment! It perhaps to make the operational cost cheaper. It is ridiculous to implant 6-cell battery into an intel core i7 machine just like this product. The result is, of course, a really poor battery life performance. It's supposed to be 12-cell battery for intel core i7 laptop, everyone knows it. The Keyboard keeps annoying me by jumping my typed texts here and there. How could that be like that? I had always trusted and bought Toshiba laptops for last ten years, yet it will be my last Toshiba laptop."

Good Laptop

POSTED BY: , Tinker AFB, OK
Overall rating: 5.0 out of 5

"I've had my laptop for the past 4 months and pratically running a lot of the new games out there. Battery life could be better but I keep mine plug to the wall. For the perfomance you're getting out of it, its not a bad tradeoff either."

Everything I need!

POSTED BY: , Charlotte, NC
Overall rating: 5.0 out of 5

"This has been the best laptop I have ever used. Super fast and tons of options. Battery life is a little on the low side but other than that, no complaints."

Keyboard is a BIG problem

POSTED BY: , Armenia,Yerevan
Overall rating: 1.0 out of 5

"My laptop is very bad in the world! Not functional keyboard "space","right SHIFT",numpad"2","+" and "4","6". SIX keys on one laptop-it's too much and the battery life is very short"

Good laptop, Terrible Battery

POSTED BY: , Ohio
Overall rating: 4.0 out of 5

"This laptop is fast and performs as well as expected, but the battery life is terrible, I am lucky to get an hour of run time when it is not plugged in."

Good System

POSTED BY: , Caldwell, ID
Overall rating: 4.0 out of 5

"I have enjoyed this system quite a bit. I would like to see a longer battery life than 1.5 hours but what can I expect when running an i7. Overall a great system and I would recommend to a friend any day."
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
Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.