Toshiba Satellite C655-S5140 Laptop

Satellite C655-S5140

MSRP: $526.99
Satellite C655-S5140 3.83 out of 5.0 based on 12 user reviews. Average Customer Rating: 3.83 out of 5.0
Read Reviews (12) 
This laptop is no longer available at most retail stores, online retailers, resellers, or ToshibaDirect.com.
We recommend taking a look at this similar line of laptops:
Satellite C850 Series »
Laptop Accessories
Shop for Satellite C655-S5140 accessories at ToshibaDirect.com.
Technical Support
Get support for your Satellite C655-S5140 or try our Laptop Forums for additional help.
Intel® Core™ i3 Processor
Accessories for the Satellite C655-S5140

Accessories
Carrying Cases
Batteries
AC Adapters
Docking & Expansion

Satellite C655-S5140 Laptop Customer Reviews

Great Value

POSTED BY:
Overall rating: 4.0 out of 5

"It's nothing fancy, but is a great value. I added a USB hub because it only had 2 USB ports. I'm not a big gamer so I didn't care that it had an integrated video card. That said it's got enough processing speed, ram and hard drive space to get most tasks done and done well, and aside from one hard drive failure it's worked perfectly for me."

An old guy sounds off!

POSTED BY: , Brunswick, GA
Overall rating: 5.0 out of 5

"I have had a desk top for years, but was always leery of joining the "Laptop Bunch." What a pleasent surprise to find the Toshiba has, while not consciously aiming at the older folks, has produced a laptop that is "senior friendly." I have invited many of my friends to observe how relatively easy it is to use the Toshiba to surf the Web and to get in contact with old friends."

Great Lap Top

POSTED BY: , Cana, Va
Overall rating: 4.0 out of 5

"Performance,and features are great. Battery life could be a bit better."

Happy with this laptop!

POSTED BY: , Charleston, SC
Overall rating: 4.0 out of 5

"The only change I would make is a way to turn off the keyboard mouse when I am using a wireless mouse. I could have used one more USB port, but that's not a major thing. Other than that, I am very please with this laptop."

1 month review

POSTED BY: , Knoxville, TN
Overall rating: 5.0 out of 5

"So far, this laptop has performed well. No hiccups at all."

POSTED BY: , Louisville, Ky.
Overall rating: 4.0 out of 5

"The computer its self is exellent.But had problems with the screan went black, sent the computer back to Toshiba they fixed it and sent it back."

Just what I needed

POSTED BY: , Summerville, SC
Overall rating: 4.0 out of 5

"Very good for my basic needs. I am not into streaming videos, gaming, etc. But, for finances, correspondence, surfing, keeping me connected while traveling, etc., it's just what I needed."

45 days old and no usb ports

POSTED BY:
Overall rating: 1.0 out of 5

"Shortest laptop life ever"

Some problems, but it works

POSTED BY: , Boston, MA
Overall rating: 3.0 out of 5

"My laptop works. I can use Microsoft Office and internet. I haven't tried the webcam yet. Problems: battery life is lower than I expected (only about 3 hours in reality, not 4 as advertised. Maybe I need to change settings.) Also, it "snores" when it sleeps. I wanted to listen to internet radio when falling asleep then hit the button to make computer sleep. Afterward it starts whirring noise even though I didn't do anything. I must manually hit "Shut down" which is annoying."

POSTED BY: , Somerset,Ma
Overall rating: 3.0 out of 5

"need more time to learn all the features"
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
Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.