Toshiba Satellite C655-S5540 Laptop

Satellite C655-S5540

MSRP: $459.99
Satellite C655-S5540 4.31 out of 5.0 based on 26 user reviews. Average Customer Rating: 4.31 out of 5.0
Read Reviews (26) 
This laptop is no longer available at most retail stores, online retailers, resellers, or ToshibaDirect.com.
We recommend taking a look at this similar line of laptops:
Satellite C850 Series »
Laptop Accessories
Shop for Satellite C655-S5540 accessories at ToshibaDirect.com.
Technical Support
Get support for your Satellite C655-S5540 or try our Laptop Forums for additional help.
Intel® Pentium® Processor
Accessories for the Satellite C655-S5540

Accessories
Carrying Cases
Batteries
AC Adapters
Docking & Expansion

Satellite C655-S5540 Laptop Customer Reviews

good stuff

POSTED BY: , rockwell nc
Overall rating: 5.0 out of 5

"i have used this machine every night since the day i bought it. ALL night! i have parkinsons and i'm disabled . Fixed income... So i value my money and must make it last. This machine is my doorway, car,starship...."

So far, so good!

POSTED BY: , memphis, tn
Overall rating: 5.0 out of 5

"I haven't used my laptop a lot yet, but so far, I've had no problems with it. I've downloaded software successfully and it is quick using the internet."

Great laptop

POSTED BY: , Conyers, GA
Overall rating: 5.0 out of 5

"I had a Toshiba laptop previously and am very happy with this brand. The Satellite C655-S5540 is very fast."

It's not great, but it's good.

POSTED BY: , Portland, OR
Overall rating: 4.0 out of 5

"This laptop came with way more bloatware than my last laptop. I don't like a lot of extra programs when I buy a laptop, but this one was a gift, so I had no say in the matter. It has ample speed and hardware for my use. It is a good looking piece of equipment too. The case is sleek, and the unit is light. Also, the fan is extremely quiet. I do not like that the touch-pad is barely discernible from the case. It's all BLACK, and difficult to detect, even when feeling around for the crack. It doesn't dip in. It doesn't have any kind of rim. This is not what killed the perfect rating for me (however). This would be a 5-star computer if it weren't for the sound. The speaker built into my cell phone is louder than the two speakers in this computer. It's so quiet, that if the fan was an average one with average sound, I wouldn't be able to hear anything coming out of the speakers. It's disappointing that I had to get attachable speakers, but the laptop was free. If I had paid for this computer myself, I'd have taken it back to the store immediately for one with better sound."

Great product.

POSTED BY: , st.louis,Mo
Overall rating: 4.0 out of 5

"Very dependable, an excellent value."

POSTED BY: , cc tx
Overall rating: 4.0 out of 5

"not bad for the price,still like xp better"

Toshibia Laptop Review

POSTED BY: , Duluth GA
Overall rating: 4.0 out of 5

"I don't like I cannot clip on an internet heading in the lower portion of the screen....I think there is a problem with the computer in that area....I have move the title to the file I want to open toward the top before it will open....otherwise just get a click, click...nothing happens."

Very Good Value for the Price

POSTED BY: , NJ
Overall rating: 4.0 out of 5

"I got this laptop as a gift and I am very happy I got this one. The overall performance and features are very impressive for the price. I am still getting use to Windows 7 and all the features. (it's much better than Vista) It is very good at surfing the web and I would definitely recommend this laptop."

luther

POSTED BY: , rockwell N.C.
Overall rating: 5.0 out of 5

"great price great laptop!"

GREAT---MAKE IT BETTER

POSTED BY:
Overall rating: 5.0 out of 5

"Happy with the product but let's make it better. Start with including a wireless mouse with all your laptops- you would be the 1st to do so-a great advertising coup. At the very least recess your adapter ports so you don't have your mouse adapter sticking out the side of the laptop contacting everything."
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
Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.