POSTED BY:
Kswa7
,
Missoula, MT
Overall rating:
4.0 out of 5
"Laptop has excellent features, large screen, software, built in web-cam, keyboard is full size and feels nice. Having a full size 10-key number pad is good. Only downside is the speakers. The max volume level is way too low. I cannot understand human speech coming out of these speakers. This is my only complaint. I recommend a seperate powered set of speakers if you are going to get this laptop. Also touchpad seems a bit twitchy sometimes, though it might be because I'm left handed."
POSTED BY:
Mrravioli
,
Pittsburgh, PA
Overall rating:
5.0 out of 5
"This laptop is a very good laptop if you are a regular person who only uses it for personal use. The only bad things i have to say about this product is that there is only 2 usb ports and the touchpad is very sensitive. I will rest my wrist on the touchpad while typing and the cursor will go crazy and sometime exit out of what i'm doing."
POSTED BY:
jackandcigar
,
West Chicago, IL
Overall rating:
5.0 out of 5
"I purchased 3 of these, one for each of my kids. They use it for online games, email, Facebook, and some homework as well. I was worried a bit with the E-300 processor and the online games, but it does just fine. Set up is easy out of the box. They love to use the webcam to talk to each other from thier rooms. It's not a high end unit but as a first laptop - it's perfect!"
POSTED BY:
Mirror
,
Melbourne, FL
Overall rating:
5.0 out of 5
"I've had literally no problems with this laptop at all. I'll admit, I was originally quite concerned because of the cheap feel of the plastic pieces but I have come to find it very durable. All I can say is great job. It does everything I need it to do without a hassle, the battery life is awesome, and it's very fast. It's everything I needed for a school and home computer. :]"
POSTED BY:
n/a
,
baton rouge la.
Overall rating:
5.0 out of 5
"i am having a good time with my laptop"
POSTED BY:
Bern
,
Rome, NY
Overall rating:
5.0 out of 5
"I went to a meeting with other professionals and all of us had a Toshiba. It was great."
POSTED BY:
Gregg
,
So. Central Missouri
Overall rating:
5.0 out of 5
"I got this over the Black Friday Weekend, 2011 and so far, I really enjoy the ease and flexibility ... I switched from a desktop to this laptop with apprehension but I haven't looked back since doing so ... My only minor complaint is it doesn't have Bluetooth but it's not a big deal ..."
POSTED BY:
Ace
,
Bloomfield NJ
Overall rating:
4.0 out of 5
"I'm a novice & am learning quite a lot on my new satallite."
POSTED BY:
storm
,
niceville
Overall rating:
3.0 out of 5
"little slower than I am used to however it is good for home use"
POSTED BY:
lscar
,
Greenville, SC
Overall rating:
4.0 out of 5
"Overall, happy with product but a few design issues that could be improved: *power cord and CD too close, have to use two hands moving cord to input/remove CD *Lots of fingerprints left on laptop itself from standard use *Volume and speakers could improve with better sound and funcionality. *One more USB port would be good for us who use a wireless mouse, so have one automatically taken"