Toshiba Satellite C675-S7200 Laptop

Satellite C675-S7200

MSRP: $466.99
Satellite C675-S7200 4.30 out of 5.0 based on 45 user reviews. Average Customer Rating: 4.30 out of 5.0
Read Reviews (45) 
This laptop is no longer available at most retail stores, online retailers, resellers, or ToshibaDirect.com.
We recommend taking a look at this similar line of laptops:
Satellite C870 Series »
Laptop Accessories
Shop for Satellite C675-S7200 accessories at ToshibaDirect.com.
Technical Support
Get support for your Satellite C675-S7200 or try our Laptop Forums for additional help.
Intel® Pentium® Processor
Accessories for the Satellite C675-S7200

Accessories
Carrying Cases
Batteries
AC Adapters
Docking & Expansion

Satellite C675-S7200 Laptop Customer Reviews

slow crashes

POSTED BY: , Maine
Overall rating: 3.0 out of 5

"This is the slowest and most trouble I've had with a computer- I don't like the photo program, I am dumped more then I like-Toshiba and Internet Explorer should get together"

Great For Gaming!!!

POSTED BY:
Overall rating: 5.0 out of 5

"I love this computer it runs The Walking Dead very nice and other games!!!!HIGHLY RECCOMEND THIS"

Love it!

POSTED BY: , New Mexico
Overall rating: 4.0 out of 5

"It's user-friendly and has everything I need on it."

Good for the price

POSTED BY:
Overall rating: 3.0 out of 5

"I have owned 4 other satellites with no real problems. But the only complaints are the speaker are kind of weak and the housing feels cheap. Overall good deal"

Highly Pleased With My Purchase!

POSTED BY: , Cedar Bluff, VA
Overall rating: 5.0 out of 5

"This is my first Toshiba laptop and also my first experience with Windows 7. I have been using my computer on a daily basis since purchasing it and have found it to be all that it was advertised to be. The laptop design is innovative, every part of it configured with mobility and ease of use in mind. It does reasonably well on battery power considering its having a 17.3" screen and being a technological powerhouse. The display is very crisp, rendering an excellent presentation of pictures and video. The laptop speakers don't offer much in the way of audio quality, but the listening experience when plugged into earbuds or into my Dolby system is phenomenal. The laptop is totally plug-and-play, quickly recognizing devices and assigning drivers to connected hardware. The touch pad is easy to use although I generally plug in a wireless mouse when doing a lot of work. Whether I'm word processing, working with audio, video, or pictures, or doing graphic design, this machine has everything that I need to get the job done. My only wish is that my Satellite had a couple more USB ports. While working on a recent project I had to unplug a device in order to connect another. It is no great inconvenience, only a little slowdown in my work process. Thanks for a great, affordable product! I will definitely be browsing Toshiba laptops again when the time comes to upgrade again."

Turned off!

POSTED BY: , York Pa.
Overall rating: 1.0 out of 5

"From the beginig laptop would crash. Bought for online classes, was ready to ship back to Toshiba for repairs then it stopped crashing. Didn't seend back as I needed it for school. Had been running trouble free for about 3 months, now crashes all the time again. Now I need to pay for telephone help."

Very good laptop

POSTED BY: , Arvada, CO
Overall rating: 4.0 out of 5

"This is my first computer of any kind. My son, who has quite a bit of PC experience, both personal and professionallly, picked this out for me and is teaching me how to use it. I don't have any base of comparison, but it has been a pleasure to learn on it & my son tells me it's a very good product."

A very good laptop...

POSTED BY: , Melbourne, FL
Overall rating: 5.0 out of 5

"Although my son had bad luck with the screen (connections) with his Toshiba laptop some years ago, he was otherwise happy with it, so I thought I would be, too. I find it works very smoothly and is very responsive to the things I want to do - mainly editing photos, handling e-mail and watching movies or TV. I bought it especially as a back up for my regular desk PC. The only drawback, which I was aware of from other reviews, is the sound is poor. So I bought an inexpensive pair of speakers and it is now perfect! I recommend it highly!"

sound

POSTED BY: , DES PLAINES IL
Overall rating: 4.0 out of 5

"when watching movies and shows on line sound is very low and hard to hear have to use head phones to hear want i'm watching"

I'm impressed

POSTED BY: , daytona Beach, FL
Overall rating: 5.0 out of 5

"My laptop is easy to use and fast. Your always there if I need support."
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
Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.