Toshiba Satellite C850-ST3NX4 Laptop

Satellite C850-ST3NX4

MSRP: $614.00
Satellite C850-ST3NX4 4.11 out of 5.0 based on 9 user reviews. Average Customer Rating: 4.11 out of 5.0
Read Reviews (9) 
This laptop is no longer available at most retail stores, online retailers, resellers, or ToshibaDirect.com.
We recommend taking a look at other Satellite C850s that are available:
Satellite C850 Series »
Laptop Accessories
Shop for Satellite C850-ST3NX4 accessories at ToshibaDirect.com.
Technical Support
Get support for your Satellite C850-ST3NX4 or try our Laptop Forums for additional help.
Intel® Core™ i3 Processor

Satellite C850-ST3NX4 Laptop Customer Reviews

Laptop

POSTED BY: , Bluffton SC
Overall rating: 5.0 out of 5

"Very easy to set up Windows 8 is a pain to get used to. But laptop works great I am very pleased. I had one ? called support and got the answer very promptly"

Great Laptop

POSTED BY: , Payette, ID
Overall rating: 4.0 out of 5

"Really good computer. However it has a lot more features and programs than I will ever use. I am just learning about computers and this one seems pretty complicated to me."

Nice Laptop but;

POSTED BY: , Eastern Washington
Overall rating: 3.0 out of 5

"The keyboard flexes too much. Makes it harder to type. It's like the outer edges are glued down which allows the center of the keyboard to flex up and down. I guess I should have order a laptop without the standard keyboard. Other than that, I like the laptop."

Great laptop Deal!

POSTED BY: , Minneapolis, MN
Overall rating: 4.0 out of 5

"The laptop is wonderful. I am not ready for Windows8, so that is a challenge.... Need to learn to takle adventage of the laptop"

defects in design

POSTED BY:
Overall rating: 4.0 out of 5

"having the power cord come out of the side of the laptop makes it hard to use and VERY EASY TO TRIP AND PULL THE COMPUTER OFF THE TABLE THE TOUCH PAD IS TOO SLICK AND MAKES MY HAND SLIP"

My New Laptop

POSTED BY: , Macon, GA
Overall rating: 3.0 out of 5

"I like my new laptop but I have had a few issues with it regarding Google Chrome and the fact that it move off screen in the middle of my typing. Other than the few setbacks it has worked great and I am so grateful to have a new laptop after going a long time without one."

Great Laptop

POSTED BY: , peoria, AZ
Overall rating: 5.0 out of 5

"Love this machine! I bought this to replace my old satellite which I was so used to, moving to this machine has been easy and I just love windows 8! Great features and such a good buy!"

Love my laptop!

POSTED BY: , Mendota, IL
Overall rating: 5.0 out of 5

"This is the second Toshiba laptop I have purchased. My other one was much smaller in memory and therefore limited usage. I enjoy the features on this one but would rather had the Windows 7 operating system. I would recommend this laptop for everyday usage!"

POSTED BY: , sarasota,fl
Overall rating: 4.0 out of 5

"great laptop for the $$$"
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
  • C850
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
Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.