Toshiba Satellite C855-S5194 Laptop

Satellite C855-S5194

MSRP: $534.99
Satellite C855-S5194 4.08 out of 5.0 based on 114 user reviews. Average Customer Rating: 4.08 out of 5.0
Read Reviews (114)  | Write Reviews
Intel® Core™ i3 Processor

Satellite C855-S5194 Laptop Customer Reviews

It is a step above average

POSTED BY: , champaign, IL
Overall rating: 4.0 out of 5

"This laptop is very versatile. I like the fact that it has usb 3.0, has an HDMI input. SD card reader. It is not too heavy. The battery life coould have been a little better. All in all it seems like a good quality product that I will enjoy for years to come."

nice

POSTED BY: , iLLINOIS
Overall rating: 5.0 out of 5

"This is my first lap top and only had it a month."

Excellent Laptop for the price

POSTED BY: , Stone Mountain, Ga
Overall rating: 5.0 out of 5

"This laptop was easy to used and price was excellent."

Best Laptop

POSTED BY:
Overall rating: 4.0 out of 5

"Happy I bought this laptop and like it better than a Dell. Will definitely be buying from toshiba in the future."

not the best laptop ever

POSTED BY: , port st lucie, fl
Overall rating: 3.0 out of 5

"lousey sound"

Best Laptop

POSTED BY: , Greenville, MS
Overall rating: 5.0 out of 5

"It is light weight, very easy to use. Cute and an excellent learning laptop for beginners because it navigates for you. Whatever project you are doing there is some type of support to help. It like a teaching tool."

POSTED BY: , Moreno Valley CA
Overall rating: 1.0 out of 5

"Disapointed!"

easiest laptop to use

POSTED BY: , Lubbock, Tx
Overall rating: 5.0 out of 5

"Like this laptop. It's better than the ones that we used at work. It's so easy and fast."

OK for the price

POSTED BY: , Atlanta
Overall rating: 4.0 out of 5

"This is not Toshiba's greatest product. Nor, is it one of their most expensive. Performance is good. Screen resolution is very good. Sound is awful. Speakers are tinny and if you are going to watch video or listen to music you'll want to add external speakers. Would I recommend this model to a friend, only after I advise them to be sure what they are buying. I would suggest an actual hands on demo before purchasing. Would I recommend Toshiba to a friend, most diffidently. OBTW, I'm not a big fan of windows 8. ."

2nd one says a lot!

POSTED BY: , Herndon VA
Overall rating: 5.0 out of 5

"I love the separate keypad and the textured touchpad. I can't get over how inexpensive this was and how much better it is than the last Toshiba I bought for 3X the price. I loved that one which is why I went back for another 6 years later but this one is even better!"
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
    Starts at: $870.99
  • L840L840
    Satellite® L840
    Great for everyday computing
    Easy to carry design
    Fashionable and affordable
    Great for enjoying multimedia
    Preloaded with Windows8
    Starts at: $449.99
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
    Starts at: $779.99
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
  • C850
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
    Starts at: $524.99
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
    Starts at: $486.99
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
    Starts at: $679.99
  • S870S870
    Satellite® S870
    Great desktop replacement
    Big screen viewing
    Premium speakers
    Entertainment-focused features
    Preloaded with Windows 8
    Starts at: $524.99

Discount Shown in Shopping Cart

Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.