Toshiba Satellite C875-S7304 Laptop

Satellite C875-S7304

MSRP: $514.99
Satellite C875-S7304 3.73 out of 5.0 based on 11 user reviews. Average Customer Rating: 3.73 out of 5.0
Read Reviews (11) 
This laptop is no longer available at most retail stores, online retailers, resellers, or ToshibaDirect.com.
We recommend taking a look at other Satellite C870s that are available:
Satellite C870 Series »
Laptop Accessories
Shop for Satellite C875-S7304 accessories at ToshibaDirect.com.
Technical Support
Get support for your Satellite C875-S7304 or try our Laptop Forums for additional help.
Intel® Core™ i3 Processor
Customize your C870 at ToshibaDirect.com

Customize

Accessories for the Satellite C875-S7304

Accessories
Carrying Cases
Batteries
AC Adapters
Docking & Expansion

Available Satellite C870 Series Laptops
C870
Model: MSRP:
C875D-S7120 $398.99
C870-ST4NX1 $399.99*
C870-ST4NX5 $429.99*
C875D-S7345 $459.99
C875D-S7105 $467.99
C875D-S7330 $499.99
C870-ST4NX2 $469.99*
C870-ST4NX3 $479.99*
C870-ST4NX4 $499.99*
C875-S7340 $619.99
C875-S7132NR $624.99
C870-BT3N11 $379.99**

*ToshibaDirect Exclusive. Price includes applicable discounts.

**Customizable laptop. Price shown is for base configuration and includes any applicable discounts. Price may change based on customization.

Satellite C875-S7304 Laptop Customer Reviews

Best Laptop ever

POSTED BY: , Amman, Jordan
Overall rating: 5.0 out of 5

"the Battery Life is the longest I used ever, No need for external fans, the performance is good, the great OS Win8 gives it a great flavor of using a great HW with a great SW."

Satellite C875-S7304 Laptop

POSTED BY: , New Jersey
Overall rating: 5.0 out of 5

"This is a very nice laptop. The only issue is windows 8. The os is really better suited for a touchscreen not a regular laptop. It would be nice if there was an easy downgrade path to win7."

quality product

POSTED BY: , shelton,ct.
Overall rating: 4.0 out of 5

"still learning"

Love Toshiba

POSTED BY: , Tucson, Arizona
Overall rating: 5.0 out of 5

"This is my second Toshiba. So far so good I am slowly learning Windows 8."

Average laptop

POSTED BY: , Iran
Overall rating: 3.0 out of 5

"Windows 8 installed on this model because the free version installed Norton Vafys very bad. The graphics card is not suitable for gaming. Windows 8 is also compatible with most software. Due to the lack of a serial number to install the new Windows 8 really got in trouble."

Lots of screen for the buck

POSTED BY: , TN
Overall rating: 3.0 out of 5

"Pros: good price for this screen size Cons: Feels cheap, keyboard wavy but works USB 3 port not identified. All port markings are on bottom of computer and not color coded. Full of crapware from Toshiba and others. Win 8 Metro GUI is lousy. I am using a Win 7 interface. In short, good price and performance for the price, but cheap all over."

Great buy

POSTED BY: , Brooklyn,ny
Overall rating: 5.0 out of 5

"I got this laptop to replace and upgrade from an old netbook and it has been easy to use and a great value for the price."

good laptop

POSTED BY: , des moines, ia
Overall rating: 5.0 out of 5

"good laptop"

Taking back

POSTED BY: , New Bremen, OH
Overall rating: 1.0 out of 5

"First start up came up (Media-failed) this was only the start. I was told to make back up disc right away! I did and it took 3 DVDs when I went to use my laptop n it wouldn't even load up, I tried to boot up from recovery disc I made and when that didn't work either I boxed it up and am taking it back tomorrow!"

excellent

POSTED BY: , Corona
Overall rating: 4.0 out of 5

"it is my first experience for this windows 8 and it is good that i have experience the same on Toshiba----leading innovation----. buy the price should be less as given. although i have got one but something should be given extra one. thanks."
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
  • C870
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
Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.