Toshiba Satellite L640-ST2N01 Laptop

Satellite L640-ST2N01

MSRP: $699.00
Satellite L640-ST2N01 4.00 out of 5.0 based on 5 user reviews. Average Customer Rating: 4.00 out of 5.0
Read Reviews (5) 
This laptop is no longer available at most retail stores, online retailers, resellers, or ToshibaDirect.com.
We recommend taking a look at this similar line of laptops:
Satellite L840 Series »
Laptop Accessories
Shop for Satellite L640-ST2N01 accessories at ToshibaDirect.com.
Technical Support
Get support for your Satellite L640-ST2N01 or try our Laptop Forums for additional help.
Intel® Core™ i3 Processor
Accessories for the Satellite L640-ST2N01

Accessories
Carrying Cases
Batteries
AC Adapters
Docking & Expansion

Satellite L640-ST2N01 Laptop Customer Reviews

Seems Good So Far

POSTED BY: , St. Louis
Overall rating: 4.0 out of 5

"The computer is good; the price is ok but not a bargain."

Seems OK

POSTED BY: , Burbank, CA
Overall rating: 4.0 out of 5

"I've had my laptop for less than a month, but so far it seems fine. My only concern is with the battery life. It shut down once with no warning, and I thought I should have had more time left. I guess I'll have to see."

Good for everyday use

POSTED BY: , Ft Lauderdale, FL
Overall rating: 3.0 out of 5

"Slightly pricier than the competition. Light weight laptop, good ergonomics, equipped with all necessary interfaces including, HDMI, Bluetooth and eSATA . Keyboard layout is nice, with no half keys, frequently used keys placed in the right position, almost like using a full desktop keyboard. function keys are well thought out and conveniently activated. Thermal design appears adequate, though I'd be careful where I place the laptop, no fallback vents in case bottom vent get blocked. Lots of useless pre-installed junk programs which can be uninstalled. I hope the battery life-expectancy is not as sub-standard as my earlier Toshiba. One MAJOR FLAW - I find the WLAN interface crashes after waking up from sleep/hibernation, at which point will not reconnect to access point and needs power cycling - happens quite often. This maybe a driver/windows issue - any fix out there yet?"

First Time Laptop

POSTED BY: , Ontario, NY
Overall rating: 5.0 out of 5

"I really enjoy my laptop and being able to sit on my couch and use it!"

Very pleased.

POSTED BY: , Lady Lake, Florida
Overall rating: 4.0 out of 5

"Overall, after 6 weeks of use, very pleased with this new laptop. It's not as solid feeling as my previous dell laptop, but so far it's more reliable. A comment: When they say "standard speakers," it is apparently code for HORRIBLE speakers. This was important to me, but I couldn't find a better solution in this price range. So I use headphones or external speakers."
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
Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.