POSTED BY:
muffinlady
,
Helena, MT
Overall rating:
4.0 out of 5
"colors are not bright and crisp but washed out like a water-color. Can barely make out detail. Very disappointing compared to my Dell computers. Sound isn't great. No instructions included on how to rectify the problems. Assumes a level of superiority which I do not possess. All-in-all, it does perform well, but the graphics are just not up to par with Dell."
POSTED BY:
kayakboy
,
Montana
Overall rating:
5.0 out of 5
"This is my first laptop, so far I am very pleased."
POSTED BY:
BAZ
,
Phoenix, AZ
Overall rating:
4.0 out of 5
"Computer is great and has all the necessary features. Memory and speed are ideal for running word processing and spreadsheet applications, reading e-mail, and using the internet. I would reconsider the screen size and would go with a 14" to 16" screen in the future. One drawback is the mouse pad- it should have edges for easier scrolling."
POSTED BY:
JP
,
Poulsbo, WA
Overall rating:
4.0 out of 5
"I was a little disappointed that the battery life was SO short- 3hrs; therefore when at home I will use the power cord but then that leaves me limited to one area- my other desktop can do that. And when I checked the price of another Toshiba battery, the price was a high. I have not had it long enough to really test the portability."